<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 adc performance</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/adc-performance/m-p/146576#M28</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hey guys,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i've a question about the adcs... in the datasheet i found that the ENOB is14.5 bits... so far so clear...&lt;/P&gt;&lt;P&gt;with a conversion time of 5us (according to another thread), is it safe to assume now that the adc can operate at 200khz sample rate with an effective resolution of 14.5 bits?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;does anybody have another source for frequency/accuracy information of the kinetis adc?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;un saludo, j&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Jul 2011 22:26:37 GMT</pubDate>
    <dc:creator>joker441</dc:creator>
    <dc:date>2011-07-05T22:26:37Z</dc:date>
    <item>
      <title>adc performance</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/adc-performance/m-p/146576#M28</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hey guys,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i've a question about the adcs... in the datasheet i found that the ENOB is14.5 bits... so far so clear...&lt;/P&gt;&lt;P&gt;with a conversion time of 5us (according to another thread), is it safe to assume now that the adc can operate at 200khz sample rate with an effective resolution of 14.5 bits?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;does anybody have another source for frequency/accuracy information of the kinetis adc?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;un saludo, j&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2011 22:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/adc-performance/m-p/146576#M28</guid>
      <dc:creator>joker441</dc:creator>
      <dc:date>2011-07-05T22:26:37Z</dc:date>
    </item>
    <item>
      <title>Re: adc performance</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/adc-performance/m-p/146577#M29</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had a similar question, so I thought I would post my analysis even though this post is getting old.&amp;nbsp; Basically, it doesn't look like you can assume that.&amp;nbsp; In order to get the 14.5 ENOB you need to use differential mode, and set the averaging to 32 samples.&amp;nbsp; I did my calculations for single ended, which gives a max ENOB of about 13.5.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For a K60-100MHz part, I can set the ADC clock to a max of 6.25Mhz because the max is 12Mhz for 16bits, and there are only power of two clock dividers.&amp;nbsp; This gives me a sample+ convert time of 140.42 usec, or about 7121 ksps.&amp;nbsp; Differential is even slower.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you get rid of the averaging you loose about a bit of ENOB and get a sample+convert time of about 6.5 usec, or about 154 ksps.&amp;nbsp; Differential will be a little bit slower again, and you can't switch between as many channels.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You will most likely need to check the DS &amp;amp; RM for the specific part and check to see what you can clock the ADC at.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 04:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/adc-performance/m-p/146577#M29</guid>
      <dc:creator>ChrisChelmecki</dc:creator>
      <dc:date>2011-12-15T04:29:31Z</dc:date>
    </item>
  </channel>
</rss>