<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: dac_adc_demo and PORTE_IDX in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/dac-adc-demo-and-PORTE-IDX/m-p/463741#M27847</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply! I believe I'm already doing that. This is my full hardware_init.c:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt; /* Enable clock for PORTs */&lt;/P&gt;&lt;P&gt;&amp;nbsp; CLOCK_SYS_EnablePortClock(PORTA_IDX);&lt;/P&gt;&lt;P&gt;&amp;nbsp; CLOCK_SYS_EnablePortClock(PORTB_IDX);&lt;/P&gt;&lt;P&gt;&amp;nbsp; CLOCK_SYS_EnablePortClock(PORTE_IDX);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Enable I2C pins */&lt;/P&gt;&lt;P&gt;&amp;nbsp; configure_i2c_pins(0);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Init board clock */&lt;/P&gt;&lt;P&gt;&amp;nbsp; BOARD_ClockInit();&lt;/P&gt;&lt;P&gt;&amp;nbsp; dbg_uart_init();&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where the configure_i2c_pins(0) is:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;void configure_i2c_pins(uint32_t instance)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; switch(instance) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; case I2C0_IDX:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* I2C0 */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTE_PCR24 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTE,24u,kPortMuxAlt5);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetOpenDrainCmd(PORTE,24u,true);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTE_PCR25 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTE,25u,kPortMuxAlt5);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetOpenDrainCmd(PORTE,25u,true);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; case I2C1_IDX:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* I2C1 */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTC_PCR10 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTC,10u,kPortMuxAlt2);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetOpenDrainCmd(PORTC,10u,true);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTC_PCR11 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTC,11u,kPortMuxAlt2);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetOpenDrainCmd(PORTC,11u,true);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; default:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tested both the dac/adc operation and i2c operation separately and they seem to work. When I try to integrate both something seems to be wrong with the i2c line. The i2c line is connected to a bluetooth module and the bluetooth module stops working when I try setting up both i2c and adc at the same time. The mcu is acting a slave for i2c. Could it be something with how I initialize the i2c slave and intialize the adc hardware? &lt;/P&gt;&lt;P&gt; I tried calling 'I2C_DRV_SlaveInit(BOARD_I2C_INSTANCE, &amp;amp;userConfig, &amp;amp;slave);' before and after I configure the adc/dac channel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 May 2016 20:46:44 GMT</pubDate>
    <dc:creator>inderjitjutla</dc:creator>
    <dc:date>2016-05-31T20:46:44Z</dc:date>
    <item>
      <title>dac_adc_demo and PORTE_IDX</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/dac-adc-demo-and-PORTE-IDX/m-p/463739#M27845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am using a MK64FN1M0VLL12 chip and I've been trying to integrate adc measurements and i2c. I've been using the dac_adc_demo as an example but I ran into some hardware initialization issues. For i2c I need to initialize the E ports:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CLOCK_SYS_EnablePortClock(PORTE_IDX);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I add that to the dac_adc_demo in hardware_init.c, the i2c line stops working. I know ADC0_SE17 shares a port with the i2c line but I'm not using that adc pin (I'm using channel 3). I'm confused as to what's causing issues with enabling the clock for port e.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 May 2016 22:24:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/dac-adc-demo-and-PORTE-IDX/m-p/463739#M27845</guid>
      <dc:creator>inderjitjutla</dc:creator>
      <dc:date>2016-05-11T22:24:23Z</dc:date>
    </item>
    <item>
      <title>Re: dac_adc_demo and PORTE_IDX</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/dac-adc-demo-and-PORTE-IDX/m-p/463740#M27846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi inderjitjutla,&lt;/P&gt;&lt;P&gt;&amp;nbsp; You just enable the PORTE clock, you should also choose the I2C pin as the I2C function, please refer to the I2C sample code configuration:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code jive_text_macro _jivemacro_uid_14630452741111450" data-renderedposition="85_8_1192_405" jivemacro_uid="_14630452741111450"&gt;&lt;/PRE&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;/* Ungate the port clock */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;CLOCK_EnableClock(kCLOCK_PortE);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;/* I2C0 pull up resistor setting */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;PORT_SetPinConfig(PORTE, 24U, &amp;amp;pinConfig);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;PORT_SetPinConfig(PORTE, 25U, &amp;amp;pinConfig);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;/* I2C0 PIN_MUX Configuration */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;PORT_SetPinMux(PORTE, 24U, kPORT_MuxAlt5);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;PORT_SetPinMux(PORTE, 25U, kPORT_MuxAlt5);&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;/* Ungate the port clock */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;CLOCK_EnableClock(kCLOCK_PortC);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;/* I2C1 pull up resistor setting */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;PORT_SetPinConfig(PORTC, 10U, &amp;amp;pinConfig);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;PORT_SetPinConfig(PORTC, 11U, &amp;amp;pinConfig);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;/* I2C1 PIN_MUX Configuration */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;PORT_SetPinMux(PORTC, 10U, kPORT_MuxAlt2);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;PORT_SetPinMux(PORTC, 11U, kPORT_MuxAlt2);&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 09:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/dac-adc-demo-and-PORTE-IDX/m-p/463740#M27846</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-05-12T09:28:03Z</dc:date>
    </item>
    <item>
      <title>Re: dac_adc_demo and PORTE_IDX</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/dac-adc-demo-and-PORTE-IDX/m-p/463741#M27847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply! I believe I'm already doing that. This is my full hardware_init.c:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt; /* Enable clock for PORTs */&lt;/P&gt;&lt;P&gt;&amp;nbsp; CLOCK_SYS_EnablePortClock(PORTA_IDX);&lt;/P&gt;&lt;P&gt;&amp;nbsp; CLOCK_SYS_EnablePortClock(PORTB_IDX);&lt;/P&gt;&lt;P&gt;&amp;nbsp; CLOCK_SYS_EnablePortClock(PORTE_IDX);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Enable I2C pins */&lt;/P&gt;&lt;P&gt;&amp;nbsp; configure_i2c_pins(0);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; /* Init board clock */&lt;/P&gt;&lt;P&gt;&amp;nbsp; BOARD_ClockInit();&lt;/P&gt;&lt;P&gt;&amp;nbsp; dbg_uart_init();&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where the configure_i2c_pins(0) is:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;void configure_i2c_pins(uint32_t instance)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; switch(instance) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; case I2C0_IDX:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* I2C0 */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTE_PCR24 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTE,24u,kPortMuxAlt5);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetOpenDrainCmd(PORTE,24u,true);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTE_PCR25 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTE,25u,kPortMuxAlt5);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetOpenDrainCmd(PORTE,25u,true);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; case I2C1_IDX:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* I2C1 */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTC_PCR10 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTC,10u,kPortMuxAlt2);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetOpenDrainCmd(PORTC,10u,true);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Affects PORTC_PCR11 register */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTC,11u,kPortMuxAlt2);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetOpenDrainCmd(PORTC,11u,true);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; default:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tested both the dac/adc operation and i2c operation separately and they seem to work. When I try to integrate both something seems to be wrong with the i2c line. The i2c line is connected to a bluetooth module and the bluetooth module stops working when I try setting up both i2c and adc at the same time. The mcu is acting a slave for i2c. Could it be something with how I initialize the i2c slave and intialize the adc hardware? &lt;/P&gt;&lt;P&gt; I tried calling 'I2C_DRV_SlaveInit(BOARD_I2C_INSTANCE, &amp;amp;userConfig, &amp;amp;slave);' before and after I configure the adc/dac channel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 May 2016 20:46:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/dac-adc-demo-and-PORTE-IDX/m-p/463741#M27847</guid>
      <dc:creator>inderjitjutla</dc:creator>
      <dc:date>2016-05-31T20:46:44Z</dc:date>
    </item>
    <item>
      <title>Re: dac_adc_demo and PORTE_IDX</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/dac-adc-demo-and-PORTE-IDX/m-p/463742#M27848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi inderjitjutla,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Did you use the I2C0 module? Did you add the external pullup in PTE24 and PTE25?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you comment the dac_adc code just leave the dac_adc initialization in the main.c function, whether your I2C can work ok?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jingjing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 05:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/dac-adc-demo-and-PORTE-IDX/m-p/463742#M27848</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-06-01T05:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: dac_adc_demo and PORTE_IDX</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/dac-adc-demo-and-PORTE-IDX/m-p/463743#M27849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;Turns out the issue was that some of the logic in the .slaveCallback function I was using in the i2c slave config. I wasn't properly handling the i2cEvent and setting the rxBuff/txBuff. My hardware was fine and the hardware_init was correct also. It was just strange because I didn't think a logic issue on the slave could disable my bluetooth lol. Your suggestion of commenting out the dac_adc code eventually led me to discover my issue. Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jun 2016 18:14:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/dac-adc-demo-and-PORTE-IDX/m-p/463743#M27849</guid>
      <dc:creator>inderjitjutla</dc:creator>
      <dc:date>2016-06-09T18:14:49Z</dc:date>
    </item>
  </channel>
</rss>