<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: MK64FX512 : VREF_OUT voltage drift</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FX512-VREF-OUT-voltage-drift/m-p/462914#M27782</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Koichi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that there is discrepancy as you said. I seems that&amp;nbsp; that the Vtdrift spec has issue, some data sheet says that the maximum of Vtdrift is 80mV instead of 15mV. You can download the data sheet of the other Kinetis K family.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Dec 2015 06:56:59 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2015-12-07T06:56:59Z</dc:date>
    <item>
      <title>MK64FX512 : VREF_OUT voltage drift</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FX512-VREF-OUT-voltage-drift/m-p/462913#M27781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We consider the VREF_OUT voltage drift.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In DataSheet Table 36. VREF full-range operating behaviors ,&lt;BR /&gt;It is described that VOUT = 1.198 V (max);( Vout Voltage reference output with factory trim at nominal VDDA and temperature= 25 °C ) .&lt;/P&gt;&lt;P&gt;&amp;nbsp; Vtdrift = 15mV ( max ) ;(Vmax -Vmin across the full temperature range)&lt;BR /&gt;&amp;nbsp; Vvdrift = 2mV ( max );(Vmax -Vmin across the full voltage range)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Next, &lt;BR /&gt;Table 38. VREF limited-range operating behaviors ,&lt;BR /&gt;It is described that VOUT = 1.225 V (max);temperature= 0 ~ 50 °C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We calculated a max case value for voltage drift.&lt;BR /&gt;1.198 + 0.015 + 0.002 = 1.215 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Question]&lt;BR /&gt;Why&amp;nbsp; is the max case value ( we&amp;nbsp; calculated) smaller than Table 38 value ?&lt;BR /&gt;1.215 &amp;lt; 1.225&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards, &lt;BR /&gt;Koichi Sakagami &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Dec 2015 02:02:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FX512-VREF-OUT-voltage-drift/m-p/462913#M27781</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2015-12-05T02:02:18Z</dc:date>
    </item>
    <item>
      <title>Re: MK64FX512 : VREF_OUT voltage drift</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FX512-VREF-OUT-voltage-drift/m-p/462914#M27782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Koichi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that there is discrepancy as you said. I seems that&amp;nbsp; that the Vtdrift spec has issue, some data sheet says that the maximum of Vtdrift is 80mV instead of 15mV. You can download the data sheet of the other Kinetis K family.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Dec 2015 06:56:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FX512-VREF-OUT-voltage-drift/m-p/462914#M27782</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-12-07T06:56:59Z</dc:date>
    </item>
  </channel>
</rss>