<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: usb stack 4.1.1</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/usb-stack-4-1-1/m-p/462208#M27721</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bruce,&lt;/P&gt;&lt;P&gt;The USB Stack 4.1.1 provide the USB_Class_CDC_Interface_CIC_Send_Data() function to implement send data from CDC class over send endpoints.&lt;/P&gt;&lt;P&gt;It can return the parameter to reflect the executing status of the function and the return parameter can remind you to reload the send buffer properly.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1880i5D233EFE17039B58/image-size/large?v=v2&amp;amp;px=999" title="2016-01-26_14-38-28.jpg" alt="2016-01-26_14-38-28.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jan 2016 06:52:38 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-01-26T06:52:38Z</dc:date>
    <item>
      <title>usb stack 4.1.1</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/usb-stack-4-1-1/m-p/462207#M27720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CDC device (KL25Z) - How can I tell when the data has gone out so that I can reload the send buffer without overwriting data that hasn't gone out yet?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jan 2016 21:06:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/usb-stack-4-1-1/m-p/462207#M27720</guid>
      <dc:creator>wba</dc:creator>
      <dc:date>2016-01-25T21:06:56Z</dc:date>
    </item>
    <item>
      <title>Re: usb stack 4.1.1</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/usb-stack-4-1-1/m-p/462208#M27721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bruce,&lt;/P&gt;&lt;P&gt;The USB Stack 4.1.1 provide the USB_Class_CDC_Interface_CIC_Send_Data() function to implement send data from CDC class over send endpoints.&lt;/P&gt;&lt;P&gt;It can return the parameter to reflect the executing status of the function and the return parameter can remind you to reload the send buffer properly.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1880i5D233EFE17039B58/image-size/large?v=v2&amp;amp;px=999" title="2016-01-26_14-38-28.jpg" alt="2016-01-26_14-38-28.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jan 2016 06:52:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/usb-stack-4-1-1/m-p/462208#M27721</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-01-26T06:52:38Z</dc:date>
    </item>
  </channel>
</rss>