<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Using OpenSDA to flash the code to custom PCB with the same microcontroller as Eval board.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-OpenSDA-to-flash-the-code-to-custom-PCB-with-the-same/m-p/462122#M27714</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Suresh Jaggal,&lt;/P&gt;&lt;P&gt;I'd like to suggest that you can follow this scenario to eliminate the debugging restriction.&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/" title="http://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/"&gt;Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jan 2016 06:14:33 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-01-26T06:14:33Z</dc:date>
    <item>
      <title>Using OpenSDA to flash the code to custom PCB with the same microcontroller as Eval board.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-OpenSDA-to-flash-the-code-to-custom-PCB-with-the-same/m-p/462121#M27713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Folks, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using OpenSDA to program the microcontroller on the other PCB. I am using FRDM-KL05Z evaluation board. The microcontoller on the custom PCB is KL05Z.&amp;nbsp;&amp;nbsp; I have rightly connected the PCB with SWD connector on the Eval board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i try to program, i receive a error stating Microcontroller mismatch.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;(Warning 17927. Target MCU mismatch. Download performance limited. See &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.pemicro.com/opensda/pe_tools.cfm" rel="nofollow"&gt;http://www.pemicro.com/opensda/pe_tools.cfm&lt;/A&gt;&lt;SPAN&gt; for information on debugging external processors.)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;My questions are.&lt;/P&gt;&lt;P&gt;1) Is it possible to flash the custom pcb with same microcontroller.&lt;/P&gt;&lt;P&gt;2) The microcontroller on the eval board has 32 pins but the microcontroller on PCB has 48 pins ( Is it a issue). The code warrior does not distinguish between these two controllers , when we start a bare board project we only have KL05Z32 where in 32 stands for 32k flash but the pins it does not specify.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jan 2016 17:47:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-OpenSDA-to-flash-the-code-to-custom-PCB-with-the-same/m-p/462121#M27713</guid>
      <dc:creator>sureshjaggal</dc:creator>
      <dc:date>2016-01-25T17:47:40Z</dc:date>
    </item>
    <item>
      <title>Re: Using OpenSDA to flash the code to custom PCB with the same microcontroller as Eval board.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-OpenSDA-to-flash-the-code-to-custom-PCB-with-the-same/m-p/462122#M27714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Suresh Jaggal,&lt;/P&gt;&lt;P&gt;I'd like to suggest that you can follow this scenario to eliminate the debugging restriction.&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/" title="http://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/"&gt;Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jan 2016 06:14:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-OpenSDA-to-flash-the-code-to-custom-PCB-with-the-same/m-p/462122#M27714</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-01-26T06:14:33Z</dc:date>
    </item>
  </channel>
</rss>