<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Pin mux tables in K60P144M150 Reference Manual and Datasheet don't show FB_CLKOUT... in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-mux-tables-in-K60P144M150-Reference-Manual-and-Datasheet-don/m-p/197778#M2743</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There has been extra functionality added to the CLK_OUT pin. It can be routed out through PTC3-ALT5. However you can now select which clock is passed out of CLK_OUT pin. It is controlled through the SIM register SOPT2. The default clock_out function is FB_CLKOUT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the flex bus with the CLKOUT pin configured for the flexbus clock.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Dec 2012 15:00:09 GMT</pubDate>
    <dc:creator>ndavies</dc:creator>
    <dc:date>2012-12-05T15:00:09Z</dc:date>
    <item>
      <title>Pin mux tables in K60P144M150 Reference Manual and Datasheet don't show FB_CLKOUT...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-mux-tables-in-K60P144M150-Reference-Manual-and-Datasheet-don/m-p/197777#M2742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the 144 pin 100MHz K60, the FB_CLKOUT signal could be muxed out on PTC3 as ALT5.&amp;nbsp; In the K60P144M150, the FB_CLKOUT doesn't appear in either the reference manual (Rev 2) or the datasheet (Rev 4).&amp;nbsp; The ref manual shows PTC3-ALT5 as undefined and the datasheet shows it as CLKOUT (as in system clock out, same as PTA6-ALT5).&amp;nbsp; Where is FB_CLKOUT now?&amp;nbsp; Are both docs wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2012 00:51:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-mux-tables-in-K60P144M150-Reference-Manual-and-Datasheet-don/m-p/197777#M2742</guid>
      <dc:creator>stevenmartin</dc:creator>
      <dc:date>2012-12-05T00:51:54Z</dc:date>
    </item>
    <item>
      <title>Re: Pin mux tables in K60P144M150 Reference Manual and Datasheet don't show FB_CLKOUT...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-mux-tables-in-K60P144M150-Reference-Manual-and-Datasheet-don/m-p/197778#M2743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There has been extra functionality added to the CLK_OUT pin. It can be routed out through PTC3-ALT5. However you can now select which clock is passed out of CLK_OUT pin. It is controlled through the SIM register SOPT2. The default clock_out function is FB_CLKOUT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the flex bus with the CLKOUT pin configured for the flexbus clock.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2012 15:00:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-mux-tables-in-K60P144M150-Reference-Manual-and-Datasheet-don/m-p/197778#M2743</guid>
      <dc:creator>ndavies</dc:creator>
      <dc:date>2012-12-05T15:00:09Z</dc:date>
    </item>
    <item>
      <title>Re: Pin mux tables in K60P144M150 Reference Manual and Datasheet don't show FB_CLKOUT...</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-mux-tables-in-K60P144M150-Reference-Manual-and-Datasheet-don/m-p/197779#M2744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven, as Norm mentioned, the FB_CLKOUT signal is assigned to pin 106 /&amp;nbsp; / PTC3, there is a small error in the device's datasheet where the pins is shown as the system CLKOUT, you can confirm the FB signal configuration in the TWR-K60F120M schematic page 4:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWR-K60F120M-SCH.pdf" title="http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWR-K60F120M-SCH.pdf"&gt;http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWR-K60F120M-SCH.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2012 18:04:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-mux-tables-in-K60P144M150-Reference-Manual-and-Datasheet-don/m-p/197779#M2744</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2012-12-11T18:04:04Z</dc:date>
    </item>
  </channel>
</rss>