<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: SPI bootload on KL43Z eval board - which SPI to use</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-bootload-on-KL43Z-eval-board-which-SPI-to-use/m-p/458384#M27381</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Arpad:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the pinmux is the same for the KL17/KL27/KL33/KL43.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Sep 2015 20:57:48 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2015-09-22T20:57:48Z</dc:date>
    <item>
      <title>SPI bootload on KL43Z eval board - which SPI to use</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-bootload-on-KL43Z-eval-board-which-SPI-to-use/m-p/458380#M27377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to bootload a KL43Z board through SPI. I was able to start the bootloader by connecting the BOOTCFG pin to the ground, and resetting the board.&lt;/P&gt;&lt;P&gt;I checked it with the debugger, and I'm sure that it booted from the ROM. I read the KL43 Sub-Family Reference Manual, and it's not clear for me that in bootload mode, which peripherals are acive at which pins.&lt;/P&gt;&lt;P&gt;I assume that somewhere there is a pin mux table that shows that which peripheral is connected to which pins after bootloader initialization.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can somebody help me in this matter?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Arpad Maroti&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 12:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-bootload-on-KL43Z-eval-board-which-SPI-to-use/m-p/458380#M27377</guid>
      <dc:creator>arep</dc:creator>
      <dc:date>2015-09-18T12:25:17Z</dc:date>
    </item>
    <item>
      <title>Re: SPI bootload on KL43Z eval board - which SPI to use</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-bootload-on-KL43Z-eval-board-which-SPI-to-use/m-p/458381#M27378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Arpad Maroti:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are sorry that the Reference Manual was not clear in this aspect. We are aware of this and will clarify it in the next revision of the manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For now here you have the correct pinout for the available peripherals in the KL43 ROM bootloader:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52211i1D79C630239923F5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies. Again our apologies for the confusion.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Sep 2015 23:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-bootload-on-KL43Z-eval-board-which-SPI-to-use/m-p/458381#M27378</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-09-20T23:38:42Z</dc:date>
    </item>
    <item>
      <title>Re: SPI bootload on KL43Z eval board - which SPI to use</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-bootload-on-KL43Z-eval-board-which-SPI-to-use/m-p/458382#M27379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your response, I was looking for exactly this table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Arpad Maroti&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2015 09:03:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-bootload-on-KL43Z-eval-board-which-SPI-to-use/m-p/458382#M27379</guid>
      <dc:creator>arep</dc:creator>
      <dc:date>2015-09-21T09:03:40Z</dc:date>
    </item>
    <item>
      <title>Re: SPI bootload on KL43Z eval board - which SPI to use</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-bootload-on-KL43Z-eval-board-which-SPI-to-use/m-p/458383#M27380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to communicate with the microcontroller on the SPI on PC4..7. We are designing our PCB with KL17s instead of KL43s. I wonder if the pinmux is the same for KL17? We are planning to use the 32-pin or the 48-pin version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Arpad Maroti&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 08:03:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-bootload-on-KL43Z-eval-board-which-SPI-to-use/m-p/458383#M27380</guid>
      <dc:creator>arep</dc:creator>
      <dc:date>2015-09-22T08:03:22Z</dc:date>
    </item>
    <item>
      <title>Re: SPI bootload on KL43Z eval board - which SPI to use</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-bootload-on-KL43Z-eval-board-which-SPI-to-use/m-p/458384#M27381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Arpad:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the pinmux is the same for the KL17/KL27/KL33/KL43.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 20:57:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-bootload-on-KL43Z-eval-board-which-SPI-to-use/m-p/458384#M27381</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-09-22T20:57:48Z</dc:date>
    </item>
  </channel>
</rss>