<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFlexbus K63 controller</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-K63-controller/m-p/457784#M27295</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;We are using&amp;nbsp; Flexbus to interface to an LCD. LCD is addressed using one bit Addr0. CS2 is used for LCD.&lt;/P&gt;&lt;P&gt;WE found that using logic analyzer. Addr0 is getting deasserted before the CS2 is getting asserted due to which LCD is not getting the Command.&lt;/P&gt;&lt;P&gt;Could some help us to identify the issue and fix the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Vinay S B&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Dec 2015 17:42:07 GMT</pubDate>
    <dc:creator>vinaysb</dc:creator>
    <dc:date>2015-12-02T17:42:07Z</dc:date>
    <item>
      <title>Flexbus K63 controller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-K63-controller/m-p/457784#M27295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;We are using&amp;nbsp; Flexbus to interface to an LCD. LCD is addressed using one bit Addr0. CS2 is used for LCD.&lt;/P&gt;&lt;P&gt;WE found that using logic analyzer. Addr0 is getting deasserted before the CS2 is getting asserted due to which LCD is not getting the Command.&lt;/P&gt;&lt;P&gt;Could some help us to identify the issue and fix the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Vinay S B&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Dec 2015 17:42:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-K63-controller/m-p/457784#M27295</guid>
      <dc:creator>vinaysb</dc:creator>
      <dc:date>2015-12-02T17:42:07Z</dc:date>
    </item>
    <item>
      <title>Re: Flexbus K63 controller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-K63-controller/m-p/457785#M27296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vinay,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please take a look on the Flexbus examples I attached to this post &lt;A _jive_internal="true" data-containerid="2019" data-containertype="14" data-content-finding="Community" data-objectid="341623" data-objecttype="1" href="https://community.nxp.com/thread/341623"&gt;FlexBus in 16 bit mode and 8 bit access&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;They are usingK60 and K70 with CW and KDS. Some of the examples use TWR.LCD. They have also a document explaining the examples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may also take a look to AN4393&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4393.pdf" title="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4393.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4393.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 22:24:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-K63-controller/m-p/457785#M27296</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2015-12-08T22:24:57Z</dc:date>
    </item>
  </channel>
</rss>