<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: K70 LCDC flicker when writing to DDR2 memory</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCDC-flicker-when-writing-to-DDR2-memory/m-p/457532#M27273</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Carl,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below thread.&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescale.jiveon.com/thread/334337" title="https://freescale.jiveon.com/thread/334337"&gt;Pixel delayed on K70 - MQX - PEG | Freescale Community&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol &lt;BR /&gt; &lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 May 2015 20:02:04 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2015-05-27T20:02:04Z</dc:date>
    <item>
      <title>K70 LCDC flicker when writing to DDR2 memory</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCDC-flicker-when-writing-to-DDR2-memory/m-p/457531#M27272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a custom board with a K70 processor connected to a TFT display (320*240*24bpp) using the LCDC controller. The LCDC reads pixel data from an 8MB DDR2 memory. I use PEG Lite and MQX 4.1. The processor is running in 120Mhz and the DDR2 memory in 150Mhz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with flicker on the display when I write to the DDR2 memory (I am not writing to the display buffer but a competely different area in the same memory). As soon as I stop writing the flicker stops.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It feels like the display controller is not able to read data from the DDR2 memory fast enough when other memory operations are performed to the same memory. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A very strange thing is that writing 32-bit data does not cause any flicker, only writing 16-bit or 8-bit data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried som ideas from this forum but nothing works:&lt;/P&gt;&lt;P&gt;* double buffer and frame-sync in PEG on/off&lt;BR /&gt;* configuring the crossbar switch priorities to give lcdc highest priority and also using round-robin scheduling&lt;BR /&gt;* flushing the caches in the display driver &lt;BR /&gt;* testing with different pixel clocks from 6 to 10Mhz for the display&lt;BR /&gt;* make sure data and instruction cache are activated&lt;BR /&gt;* activating burst-mode for lcdc transfers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea what could cause a problem like this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 May 2015 11:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCDC-flicker-when-writing-to-DDR2-memory/m-p/457531#M27272</guid>
      <dc:creator>carl-magnusmoon</dc:creator>
      <dc:date>2015-05-23T11:01:43Z</dc:date>
    </item>
    <item>
      <title>Re: K70 LCDC flicker when writing to DDR2 memory</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCDC-flicker-when-writing-to-DDR2-memory/m-p/457532#M27273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Carl,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below thread.&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescale.jiveon.com/thread/334337" title="https://freescale.jiveon.com/thread/334337"&gt;Pixel delayed on K70 - MQX - PEG | Freescale Community&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol &lt;BR /&gt; &lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2015 20:02:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCDC-flicker-when-writing-to-DDR2-memory/m-p/457532#M27273</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-05-27T20:02:04Z</dc:date>
    </item>
  </channel>
</rss>