<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FRDM-KL26Z development board: are the two possible TPM interrupts individual?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL26Z-development-board-are-the-two-possible-TPM-interrupts/m-p/457286#M27262</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gabriel Flueran:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The two interrupts are independent, so they both can be activated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually the interrupt vector is the same, so the interrupt handler must be shared and you need to check the flags to see which interrupt triggered.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Aug 2015 17:25:08 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2015-08-24T17:25:08Z</dc:date>
    <item>
      <title>FRDM-KL26Z development board: are the two possible TPM interrupts individual?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL26Z-development-board-are-the-two-possible-TPM-interrupts/m-p/457285#M27261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently working on a FRDM-KL26Z development board&amp;nbsp; and trying to implement an input signal's Dutycycle measurement using the INPUT CAPTURE function of a TPM. However, the same TPM may have some channels configured for PWM signal generation in the meantime, using its EPWM function.&lt;BR /&gt;By my question I mean, if I set the TOIE flag and a CHnIE flag, will both of the interrupts (timer overflow &amp;amp; channel interrupt) be generated and possibly be treated in the same handler? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance for your responses.&lt;BR /&gt;Gabi F&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 08:42:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL26Z-development-board-are-the-two-possible-TPM-interrupts/m-p/457285#M27261</guid>
      <dc:creator>gabrielflueran</dc:creator>
      <dc:date>2015-08-21T08:42:57Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL26Z development board: are the two possible TPM interrupts individual?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL26Z-development-board-are-the-two-possible-TPM-interrupts/m-p/457286#M27262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gabriel Flueran:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The two interrupts are independent, so they both can be activated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually the interrupt vector is the same, so the interrupt handler must be shared and you need to check the flags to see which interrupt triggered.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2015 17:25:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL26Z-development-board-are-the-two-possible-TPM-interrupts/m-p/457286#M27262</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-08-24T17:25:08Z</dc:date>
    </item>
  </channel>
</rss>