<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Using USB CDC causes a Watchdog Interrupt</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-USB-CDC-causes-a-Watchdog-Interrupt/m-p/457146#M27255</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Coleman Moore,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which version of the USB stack you are using? Would you please provide more details of the demo run on your board? Thanks for your patience!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Sep 2015 07:13:21 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2015-09-17T07:13:21Z</dc:date>
    <item>
      <title>Using USB CDC causes a Watchdog Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-USB-CDC-causes-a-Watchdog-Interrupt/m-p/457145#M27254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the USB CDC with the k22f12810 part and after 10-15 writes of data using "USB_Class_CDC_Send_Data()" the program stops at the watchdog interrupt.&amp;nbsp; The watchdog is disabled at the beginning of the program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Coleman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 01:05:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-USB-CDC-causes-a-Watchdog-Interrupt/m-p/457145#M27254</guid>
      <dc:creator>colemanmoore</dc:creator>
      <dc:date>2015-09-17T01:05:33Z</dc:date>
    </item>
    <item>
      <title>Re: Using USB CDC causes a Watchdog Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-USB-CDC-causes-a-Watchdog-Interrupt/m-p/457146#M27255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Coleman Moore,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which version of the USB stack you are using? Would you please provide more details of the demo run on your board? Thanks for your patience!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Sep 2015 07:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-USB-CDC-causes-a-Watchdog-Interrupt/m-p/457146#M27255</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2015-09-17T07:13:21Z</dc:date>
    </item>
  </channel>
</rss>