<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FRDM-KL25Z - Cant load precompiled examples</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197306#M2723</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;do you use any windows explorer extensions? I have seen cases where such extensions affect the file copied. Can you try to copy the file using the command/DOS prompt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Dec 2012 04:49:20 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2012-12-05T04:49:20Z</dc:date>
    <item>
      <title>FRDM-KL25Z - Cant load precompiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197305#M2722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The title might be completely wrong, but I'm going to explain what I can and cant do and hopefully it will make sense.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I plug the board in using the SDA usb port. A virtual com port enumerates as a "OpenSDA - CDC Serial Port" (v1.1.2600.1). I also have v11.1.0.0 of Jungo installed. I dont have the PEMicro OpenSDA Debug Driver installed. A flash drive ("FRDM-KL25Z") appears with a couple of HTML files, some driver info, and a LASTSTAT.txt. &lt;/P&gt;&lt;P&gt;No software seems to be running on the Freescale ARM - no LEDs are flashing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I cycle the power holding the reset button, then the green LED flashes, and a flash drive "BOOTLOADER" appears. I copy "DEBUG-APP_Pemicro_v102" into the drive and cycle the power again. I dont get any prompts for the PEMicro OpenSDA Debug Driver.&lt;/P&gt;&lt;P&gt;Going back into BOOTLOADER, I load the "MSD-FRDM-KL25Z_Pemicro_v105" back into the device. Next I go into BOOTLOADER and try copying the *.srec files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But nothing I do gets the tricoloured LED back up and flashing, or installs the OpenSDA debug drivers.&lt;/P&gt;&lt;P&gt;Am I doing something drastically wrong, and how can I get it back to the world of the living?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've installed CodeWarrior 10.3 Beta and would desperately like to start some development. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Stephen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2012 20:33:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197305#M2722</guid>
      <dc:creator>stephenhewitson</dc:creator>
      <dc:date>2012-12-04T20:33:28Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z - Cant load precompiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197306#M2723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;do you use any windows explorer extensions? I have seen cases where such extensions affect the file copied. Can you try to copy the file using the command/DOS prompt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2012 04:49:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197306#M2723</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-12-05T04:49:20Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z - Cant load precompiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197307#M2724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have no idea how mad that was driving me. Is this just because I was using TeraCopy?&lt;/P&gt;&lt;P&gt;Thanks again for your quick response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stephen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2012 06:54:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197307#M2724</guid>
      <dc:creator>stephenhewitson</dc:creator>
      <dc:date>2012-12-05T06:54:42Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z - Cant load precompiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197308#M2725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stephen,&lt;/P&gt;&lt;P&gt;do you say it is working now (with the DOS/cmd prompt)?&lt;/P&gt;&lt;P&gt;So yes, it seems using 'special' utilities like TeraCopy or other File extensions have an impact how the data is transmitted. And it seems like the OpenSDA bootloader has issues with it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2012 06:58:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197308#M2725</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-12-05T06:58:50Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z - Cant load precompiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197309#M2726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using the command prompt worked for me. Presumably the issue on the k20 can't be fixed without new code and a jtag programmer. Just thinking out loud, would it be possible to use a second freedom board to reprogram the opensda debugger on the k20&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sent from Samsung Mobile&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2012 13:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197309#M2726</guid>
      <dc:creator>stephenhewitson</dc:creator>
      <dc:date>2012-12-05T13:57:06Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z - Cant load precompiled examples</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197310#M2727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stephen,&lt;/P&gt;&lt;P&gt;no, the K20 cannot be re-programmed, as it is secured with mass erase disabled. See&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/305229"&gt;Use removed MK20 part from freedom board&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2012 14:40:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-Cant-load-precompiled-examples/m-p/197310#M2727</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-12-05T14:40:57Z</dc:date>
    </item>
  </channel>
</rss>