<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: How to configure SDHC module?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456581#M27208</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to enable the clock in SDHC-&amp;gt;SYSCTL (SDCLKEN) before clocks are sent when INITA mask is set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Normally the 4 bit mode is set only after the initialisation sequence has completed and the bus width programmed in the SD card (bus width command CMD6).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis.html" rel="nofollow"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;K64: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/FRDM-K64F.html" rel="nofollow"&gt;µTasker Kinetis FRDM-K64F support&lt;/A&gt;&amp;nbsp; / &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/TWR-K64F120M.html" rel="nofollow"&gt;µTasker Kinetis TWR-K64F120M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market &lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Aug 2015 15:48:06 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2015-08-21T15:48:06Z</dc:date>
    <item>
      <title>How to configure SDHC module?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456578#M27205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;​hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to configure the SDHC module, but I seem to be getting an ISR Default?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I Activated the clock gating, then I try to setup the PTE PORTS (0 - 5) and turn them to mux(4), but as I&lt;/P&gt;&lt;P&gt;step through the code, every time I step over PTE1 I get the ISR Default???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can someone explain how to setup the SDHC? Im not using PE and I would like to interface with an SD micro.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 02:48:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456578#M27205</guid>
      <dc:creator>neilporven</dc:creator>
      <dc:date>2015-08-21T02:48:14Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure SDHC module?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456579#M27206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I found out that, although, I would like to use the SDHC module and activating the clock gating for it like so:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// Enable Clock to SDHC&lt;/P&gt;&lt;P&gt;SIM_SCGC3 |= SIM_SCGC3_SDHC_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not the only thing that needs to be done!&amp;nbsp; The issue I was having when I tried to multiplex PORTE is because, I also needed to &lt;/P&gt;&lt;P&gt;activate the clock gating for PORTE like so,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIM_SCGC5 |= SIM_SCGC5_PORTE_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I was able to multiplex the lines:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; PORTE_PCR0 = PORT_PCR_MUX(4); //PTE0&lt;/P&gt;&lt;P&gt; PORTE_PCR1 = PORT_PCR_MUX(4); //PTE1&lt;/P&gt;&lt;P&gt; PORTE_PCR2 = PORT_PCR_MUX(4); //PTE2&lt;/P&gt;&lt;P&gt; PORTE_PCR3 = PORT_PCR_MUX(4); //PTE3&lt;/P&gt;&lt;P&gt; PORTE_PCR4 = PORT_PCR_MUX(4); //PTE4&lt;/P&gt;&lt;P&gt; PORTE_PCR5 = PORT_PCR_MUX(4); //PTE5&lt;/P&gt;&lt;P&gt; PORTE_PCR5 = PORT_PCR_MUX(4); //PTE6&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I set the mode for the SD:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDHC-&amp;gt;PROCTL |= SDHC_PROCTL_DTW(0x01); //Data Transfer Width (01b 4-bit mode)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but, when I tried to do this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDHC-&amp;gt;SYSCTL |= SDHC_SYSCTL_INITA_MASK; //When this bit is set, 80 SD-clocks are sent to the card&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't see the 80 SD-clocks?&amp;nbsp; Is there some other register in/out of the SDHC that needs to be set?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 14:35:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456579#M27206</guid>
      <dc:creator>neilporven</dc:creator>
      <dc:date>2015-08-21T14:35:44Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure SDHC module?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456580#M27207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, so apparently I don't know how to use my scope......&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 80 SD-clocks are there, but If anyone see an issue with what I am doing above and possibly missing something please &lt;/P&gt;&lt;P&gt;add your comments.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 15:44:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456580#M27207</guid>
      <dc:creator>neilporven</dc:creator>
      <dc:date>2015-08-21T15:44:12Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure SDHC module?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456581#M27208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to enable the clock in SDHC-&amp;gt;SYSCTL (SDCLKEN) before clocks are sent when INITA mask is set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Normally the 4 bit mode is set only after the initialisation sequence has completed and the bus width programmed in the SD card (bus width command CMD6).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis.html" rel="nofollow"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;K64: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/FRDM-K64F.html" rel="nofollow"&gt;µTasker Kinetis FRDM-K64F support&lt;/A&gt;&amp;nbsp; / &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/TWR-K64F120M.html" rel="nofollow"&gt;µTasker Kinetis TWR-K64F120M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market &lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 15:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456581#M27208</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-08-21T15:48:06Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure SDHC module?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456582#M27209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that SDHC-&amp;gt;SYSCTL(SDCLKEN) is enabled from reset, either way I made sure to set it, it doesn't hurt:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDHC-&amp;gt;SYSCTL |= SDHC_SYSCTL_SDCLKEN_MASK; //Make sure SD Clock is Enabled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to figure out how to send a command, it looks like SDHC-&amp;gt;CMDARG is the register I need, but how do I &lt;/P&gt;&lt;P&gt;give it say CMD0?&amp;nbsp; The short initialization/application note its not clear....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 17:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456582#M27209</guid>
      <dc:creator>neilporven</dc:creator>
      <dc:date>2015-08-21T17:08:34Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure SDHC module?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456583#M27210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Neil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the clock is enabled out of reset. Since it needs to be disabled each time the speed is changed (eg. when moving from 400kHz to the final operating speed) it is generally re-enabled at similar code points. You may want to also check that you initially use the mandatory 100kHz..400kHz when sending the clocks and the first commands.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To send CMD0&lt;/P&gt;&lt;P&gt;- you need first to wait for the 80 clocks to complete (SDHC_SYSCTL_INITA_MASK is self-clearing and so can be monitored for this).&lt;/P&gt;&lt;P&gt;- Wait for idle line (using PRSSTAT).&lt;/P&gt;&lt;P&gt;- Write the argument to SDHC_CMDARG (0x00000000 in this case)&lt;/P&gt;&lt;P&gt;- Lauch the command by writing to XFERTYP (0x00020000) in this case&lt;/P&gt;&lt;P&gt;- Wait for the command to complete by monitoring IRQSTAT (CC wil be set to '1')&lt;/P&gt;&lt;P&gt;- Reset flags in IRQSTAT (for next use)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then continue with the standard SD card initialisation sequence, including moving to 4-bit operating mode, followed by mouting its FAT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 20:16:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456583#M27210</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-08-21T20:16:08Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure SDHC module?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456584#M27211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Mark, is there documentation on this (besides what is in the K64 Sub-Family Reference Manual)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 20:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456584#M27211</guid>
      <dc:creator>neilporven</dc:creator>
      <dc:date>2015-08-21T20:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure SDHC module?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456585#M27212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Neil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is best to use the document in the Kinetis part manual together with reference code that already operates with the SDHC. Some details may need to be worked out with some trial and error - also read the chip errata since there tend to be a couple of SDHC issues to be aware of.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SDHC layer is also only the lowest layer in the protocoll so you may need to study the SD group's Physical Layer specification and also FAT specification, assuming you need to work with the SD card as FAT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Freescale examples have SDHC driver and FatsFS.&lt;/P&gt;&lt;P&gt;- I use the uTasker SDHC driver and utFAT, which allows the SD card, SDHC and FAT operation to be simulated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis.html" rel="nofollow"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;K64: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/FRDM-K64F.html" rel="nofollow"&gt;µTasker Kinetis FRDM-K64F support&lt;/A&gt;&amp;nbsp; / &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/TWR-K64F120M.html" rel="nofollow"&gt;µTasker Kinetis TWR-K64F120M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;utFAT: &lt;A href="http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF" title="http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF"&gt;http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market &lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Aug 2015 21:12:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456585#M27212</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-08-21T21:12:31Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure SDHC module?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456586#M27213</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an issue using Freescale's SDHC driver and FatsFS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Neil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 01:47:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456586#M27213</guid>
      <dc:creator>neilporven</dc:creator>
      <dc:date>2015-09-09T01:47:56Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure SDHC module?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456587#M27214</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Neil&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I doubt that there is a problem since SDHC and FAT layers are usually totally independent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis.html" rel="nofollow"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;K64: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/FRDM-K64F.html" rel="nofollow"&gt;µTasker Kinetis FRDM-K64F support&lt;/A&gt;&amp;nbsp; / &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/TWR-K64F120M.html" rel="nofollow"&gt;µTasker Kinetis TWR-K64F120M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;utFAT: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF" rel="nofollow"&gt;http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market &lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 12:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456587#M27214</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-09-09T12:25:51Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure SDHC module?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456588#M27215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Mark.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 16:12:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-configure-SDHC-module/m-p/456588#M27215</guid>
      <dc:creator>neilporven</dc:creator>
      <dc:date>2015-09-09T16:12:18Z</dc:date>
    </item>
  </channel>
</rss>