<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: meterlib1ph_cfg I_MAX, U_MAX?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/meterlib1ph-cfg-I-MAX-U-MAX/m-p/455786#M27163</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The U_MAX has two factors could affect that value, one is the meter AC_DC SMPS related circuit design, which should match with the meter spec design requirement, the other one to meet the current measurement requirement.&lt;/P&gt;&lt;P&gt;The I_MAX value is based on hardware design and the ADC measure range (VREFH voltage), the ADC measurement value should not exceed the measure range to make current value in a range. The hardware schematics (shunt resistor value) also affect the I_MAX value, which also affect the U_MAX value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Aug 2015 05:44:48 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2015-08-26T05:44:48Z</dc:date>
    <item>
      <title>meterlib1ph_cfg I_MAX, U_MAX?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/meterlib1ph-cfg-I-MAX-U-MAX/m-p/455785#M27162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;My project is based on _twr_emeter_demo(old one with KM34 128 series).&lt;/P&gt;&lt;P&gt;I can see a document: &lt;SPAN style="line-height: 1.5;"&gt;DRM143 Kinetis-M One-Phase Power Meter Reference Design.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the question details.&lt;/P&gt;&lt;P&gt;Does U_MAX and I_MAX come from this schematic?&lt;/P&gt;&lt;P&gt;Then U_MAX should be 325.26V as it mentioned?&lt;/P&gt;&lt;P&gt;However, on page 25, it mentioned:286V not 325.26V.&lt;/P&gt;&lt;P&gt;I am not sure which value is correct one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If my circuit use smaller register values such as two 150 Kohm instead of four 150 Kohm, then U_MAX value should be changed? then how?&lt;/P&gt;&lt;P&gt;There is no note about I_MAX though. Anyone know how to pick the value?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hyunwoo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; - page 25,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52638i65ABC959F172309E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; - page 13,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52598iBF0D70B8B7C601C0/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2015 22:15:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/meterlib1ph-cfg-I-MAX-U-MAX/m-p/455785#M27162</guid>
      <dc:creator>hyunwoochoi</dc:creator>
      <dc:date>2015-08-20T22:15:07Z</dc:date>
    </item>
    <item>
      <title>Re: meterlib1ph_cfg I_MAX, U_MAX?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/meterlib1ph-cfg-I-MAX-U-MAX/m-p/455786#M27163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The U_MAX has two factors could affect that value, one is the meter AC_DC SMPS related circuit design, which should match with the meter spec design requirement, the other one to meet the current measurement requirement.&lt;/P&gt;&lt;P&gt;The I_MAX value is based on hardware design and the ADC measure range (VREFH voltage), the ADC measurement value should not exceed the measure range to make current value in a range. The hardware schematics (shunt resistor value) also affect the I_MAX value, which also affect the U_MAX value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2015 05:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/meterlib1ph-cfg-I-MAX-U-MAX/m-p/455786#M27163</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-08-26T05:44:48Z</dc:date>
    </item>
  </channel>
</rss>