<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Info on K70</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Info-on-K70/m-p/454165#M27046</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sudeep,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as you can see in the Reference Manual you have the option to use Multiplexed 32-bit address and 32-bit data. Therefore you can address 2^32 bytes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Nov 2015 21:02:52 GMT</pubDate>
    <dc:creator>Carlos_Musich</dc:creator>
    <dc:date>2015-11-05T21:02:52Z</dc:date>
    <item>
      <title>Info on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Info-on-K70/m-p/454164#M27045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Can anyone please tell me what is the maximum size of external flash that can be connected to K70 and also the source from where this info was taken&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;P&gt;Sudeep&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Nov 2015 05:10:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Info-on-K70/m-p/454164#M27045</guid>
      <dc:creator>sudeepaithal</dc:creator>
      <dc:date>2015-11-04T05:10:17Z</dc:date>
    </item>
    <item>
      <title>Re: Info on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Info-on-K70/m-p/454165#M27046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sudeep,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;as you can see in the Reference Manual you have the option to use Multiplexed 32-bit address and 32-bit data. Therefore you can address 2^32 bytes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Nov 2015 21:02:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Info-on-K70/m-p/454165#M27046</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2015-11-05T21:02:52Z</dc:date>
    </item>
  </channel>
</rss>