<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K60 hardware question</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453529#M26978</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears my probing methods were too primitive as we don't&lt;BR /&gt;have a header that will mate with J8. Can you confirm my&lt;BR /&gt;measurement that these sockets have contacts on 2 mm&lt;BR /&gt;centers and accept 0.5 mm pins? (I intend to buy some.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FWIW: I got SW2 to work some time ago with no problems.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Dec 2015 09:53:27 GMT</pubDate>
    <dc:creator>garylynch</dc:creator>
    <dc:date>2015-12-01T09:53:27Z</dc:date>
    <item>
      <title>K60 hardware question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453525#M26974</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a question regarding K60 hardware.&amp;nbsp; Is there a forum for that? (I can't find one.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Nov 2015 14:27:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453525#M26974</guid>
      <dc:creator>garylynch</dc:creator>
      <dc:date>2015-11-30T14:27:20Z</dc:date>
    </item>
    <item>
      <title>Re: K60 hardware question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453526#M26975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can reply here with your question, I have moved your question to the correct forum. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Nov 2015 15:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453526#M26975</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2015-11-30T15:48:22Z</dc:date>
    </item>
    <item>
      <title>Re: K60 hardware question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453527#M26976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I have a TWR-K60D100M-KIT tower system with K60 MCU. I am writing simple test programs and just tried to connect a bunch of switches to 8 pins I configured as inputs on port C. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am accessing it via J8 on the primary side elevator board. I wired it by the provided schematic:&lt;/P&gt;&lt;P&gt;- PTC0 J8-66&lt;BR /&gt;- PTC1 J8-67&lt;BR /&gt;- PTC2 J8-68&lt;BR /&gt;- PTC3 J8-64&lt;BR /&gt;- PTC4 J8-69&lt;BR /&gt;- PTC5 J8-70&lt;BR /&gt;- PTC6 J8-71&lt;BR /&gt;- PTC7 J8-72&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;configured each pin as input, enabled open drain and pull-up resistors. I then threw my switches and read the results back via the KDS debugger, looking at GPIOC_PDIR. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bits seem to be scrambled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible my schematic does not match my board? If there are revision numbers on the schematic and the board, how do I find and interpret them? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Writing this makes me realize that 'open-drain' is a property of an output and is irrelevant to this application. This begs the question whether there are combinations of irrelevant fields in the PCRs that cause problems. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can find no hint of this in the reference manual, however.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Nov 2015 16:02:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453527#M26976</guid>
      <dc:creator>garylynch</dc:creator>
      <dc:date>2015-11-30T16:02:41Z</dc:date>
    </item>
    <item>
      <title>Re: K60 hardware question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453528#M26977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary,&lt;/P&gt;&lt;P&gt;I'd like to suggest that you can use the multimeter to check that whether the schematic match the board or not.&lt;/P&gt;&lt;P&gt;On the board, you can find the tags that illustrate the sch version.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="IMG_20151201_100944.jpg"&gt;&lt;IMG alt="IMG_20151201_100944.jpg" src="https://community.nxp.com/t5/image/serverpage/image-id/51981iA22BDF6F758E786C/image-size/large?v=v2&amp;amp;px=999" title="IMG_20151201_100944.jpg" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="IMG_20151201_101005.jpg"&gt;&lt;IMG alt="IMG_20151201_101005.jpg" src="https://community.nxp.com/t5/image/serverpage/image-id/52015i4A1155A27836BE77/image-size/large?v=v2&amp;amp;px=999" title="IMG_20151201_101005.jpg" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;For the SW2 which connects the PTE26 on the TWR-K60D100M board, it's available to configure the PTE26 as below.&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code jive_text_macro _jivemacro_uid_14489355955892110" data-renderedposition="1276_8_1232_32" jivemacro_uid="_14489355955892110" modifiedtitle="true"&gt;&lt;P&gt;&amp;nbsp; PORTE_PCR26=PORT_PCR_MUX(1)|PORT_PCR_IRQC(0xA)|PORT_PCR_PE_MASK|PORT_PCR_PS_MASK;&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 13:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453528#M26977</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2020-11-02T13:22:50Z</dc:date>
    </item>
    <item>
      <title>Re: K60 hardware question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453529#M26978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears my probing methods were too primitive as we don't&lt;BR /&gt;have a header that will mate with J8. Can you confirm my&lt;BR /&gt;measurement that these sockets have contacts on 2 mm&lt;BR /&gt;centers and accept 0.5 mm pins? (I intend to buy some.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FWIW: I got SW2 to work some time ago with no problems.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Dec 2015 09:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453529#M26978</guid>
      <dc:creator>garylynch</dc:creator>
      <dc:date>2015-12-01T09:53:27Z</dc:date>
    </item>
    <item>
      <title>Re: K60 hardware question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453530#M26979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary,&lt;/P&gt;&lt;P&gt;The dimension illustrates as below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="265114199918367197.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53077i467FF15B36109F5F/image-size/large?v=v2&amp;amp;px=999" role="button" title="265114199918367197.jpg" alt="265114199918367197.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Dec 2015 06:41:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-hardware-question/m-p/453530#M26979</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-12-04T06:41:02Z</dc:date>
    </item>
  </channel>
</rss>