<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Driving LED martix with K70</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driving-LED-martix-with-K70/m-p/450806#M26718</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you could use K70 DSPI module works with LED drive IC.&lt;/P&gt;&lt;P&gt;If customer want to use two data output line, I would recommend customer to use two DSPI modules.&lt;/P&gt;&lt;P&gt;The Max. DSPI baud rate could up to 30Mbps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Nov 2015 04:56:25 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2015-11-30T04:56:25Z</dc:date>
    <item>
      <title>Driving LED martix with K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driving-LED-martix-with-K70/m-p/450805#M26717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a 16 by 96 red/green LEd display panel, that I need to drive from a K70 processor (actually a Kinetis K-70-SOM board). I'm hoping some of you can suggest the best way to do this?&lt;BR /&gt;The display is driven by two 96-bit shift registers with latches (one for red, one for green), so I need to shift 96 bits into each register, latch the data into the drivers, and then repeat for each column on the display. Some questions:&lt;BR /&gt; - Can I use the K70's SPI interface for doing this? The display interface is not explicitly an SPI interface, but it is very similar.&lt;BR /&gt; - Can I drive two data bits with the same clock using the SPI interface?&lt;BR /&gt; - How fast can the K70 load the serial shift register?&lt;/P&gt;&lt;P&gt;Thanks for your help - Rowan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Nov 2015 18:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driving-LED-martix-with-K70/m-p/450805#M26717</guid>
      <dc:creator>rowans-b</dc:creator>
      <dc:date>2015-11-27T18:46:15Z</dc:date>
    </item>
    <item>
      <title>Re: Driving LED martix with K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driving-LED-martix-with-K70/m-p/450806#M26718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you could use K70 DSPI module works with LED drive IC.&lt;/P&gt;&lt;P&gt;If customer want to use two data output line, I would recommend customer to use two DSPI modules.&lt;/P&gt;&lt;P&gt;The Max. DSPI baud rate could up to 30Mbps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Nov 2015 04:56:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driving-LED-martix-with-K70/m-p/450806#M26718</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-11-30T04:56:25Z</dc:date>
    </item>
  </channel>
</rss>