<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: What does pin function name with _b suffix specify?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-pin-function-name-with-b-suffix-specify/m-p/448801#M26572</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jonathan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;_b means that it is negative logic (eg. RESET_b is reset with a '0', or UART3_RTS_b asserts to '0'). Others will "tend" to be positive logic (asserts to '1' or react to '1' at input).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Oct 2015 15:56:00 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2015-10-09T15:56:00Z</dc:date>
    <item>
      <title>What does pin function name with _b suffix specify?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-pin-function-name-with-b-suffix-specify/m-p/448800#M26571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Some Kinetis pin functions have a _b suffix.&amp;nbsp; There's the RESET_b pin, but also others such as UART0_CTS_b.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried searching datasheet and user manual but can't seem to find out what this indicates.&amp;nbsp; Of course there are 100's of matches on _b so I may have missed it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 15:38:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-pin-function-name-with-b-suffix-specify/m-p/448800#M26571</guid>
      <dc:creator>rev</dc:creator>
      <dc:date>2015-10-09T15:38:51Z</dc:date>
    </item>
    <item>
      <title>Re: What does pin function name with _b suffix specify?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-pin-function-name-with-b-suffix-specify/m-p/448801#M26572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jonathan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;_b means that it is negative logic (eg. RESET_b is reset with a '0', or UART3_RTS_b asserts to '0'). Others will "tend" to be positive logic (asserts to '1' or react to '1' at input).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 15:56:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-pin-function-name-with-b-suffix-specify/m-p/448801#M26572</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-10-09T15:56:00Z</dc:date>
    </item>
    <item>
      <title>Re: What does pin function name with _b suffix specify?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-pin-function-name-with-b-suffix-specify/m-p/448802#M26573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, of course, silly me!&amp;nbsp; What threw me was that some ADC signals also have a 'b' suffix.&amp;nbsp; Now clearly that means the alternate location since there are ADC signals with 'a' suffix also.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 16:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-pin-function-name-with-b-suffix-specify/m-p/448802#M26573</guid>
      <dc:creator>rev</dc:creator>
      <dc:date>2015-10-09T16:27:09Z</dc:date>
    </item>
    <item>
      <title>Re: What does pin function name with _b suffix specify?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-pin-function-name-with-b-suffix-specify/m-p/448803#M26574</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the ADCs have a mux which allows their channel input to be set to either Mux a or Mux b position (although some packages don't support both and in this case there is neither _a nor _b).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 16:45:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-pin-function-name-with-b-suffix-specify/m-p/448803#M26574</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-10-09T16:45:07Z</dc:date>
    </item>
  </channel>
</rss>