<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: JTAG connections in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-connections/m-p/446978#M26418</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Luiz, I use a Segger J-Link with the K22F and K64F which also has a 20pin connector.&amp;nbsp; However, there is a 10pin Cortex-M adapter that plugs into the hardware and then has a 10pin ribbon connection.&amp;nbsp; So you likely really only need these connections.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30810iD01FD63285B7F8A0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 May 2015 15:36:31 GMT</pubDate>
    <dc:creator>dave408</dc:creator>
    <dc:date>2015-05-22T15:36:31Z</dc:date>
    <item>
      <title>JTAG connections</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-connections/m-p/446975#M26415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using MK22FN1M0VLQ12 . What are the minimum signals needed for JTAG connection ?&lt;/P&gt;&lt;P&gt;We plan to use PEMICRO Multilink Universal ( 20-pin connector ). Where can I find this information ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Luiz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2015 19:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-connections/m-p/446975#M26415</guid>
      <dc:creator>pasini</dc:creator>
      <dc:date>2015-05-19T19:57:33Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG connections</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-connections/m-p/446976#M26416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luiz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check Kinetis K family product debug interface at chapter 2.1.5.3 of &amp;lt;&amp;lt;&lt;A href="http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf"&gt;Kinetis Peripheral Module Quick Reference&lt;/A&gt;&amp;gt;&amp;gt;&lt;/P&gt;&lt;P&gt;It also could refer K22 product JTAG debugger circuit of &lt;A href="http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWR-K22F120M-SCH.pdf"&gt;TWR-K22F120M board schematics&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 02:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-connections/m-p/446976#M26416</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-05-20T02:34:34Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG connections</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-connections/m-p/446977#M26417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Luiz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K22 has several debug interfaces as below. For minimum debug signals, SWD is recommended unless JTAG is mendatody.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24801iF8C83BE0A84A7288/image-size/large?v=v2&amp;amp;px=999" title="Debug.JPG" alt="Debug.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your use of Multilink Universal, the attachement can help. Please look into connector chapter then you can find info.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25197i73878DDBFAC16857/image-size/large?v=v2&amp;amp;px=999" title="Connections 1.JPG" alt="Connections 1.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25415i07348C0C865C64A2/image-size/large?v=v2&amp;amp;px=999" title="Connections 2.JPG" alt="Connections 2.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Thomas Kang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2015 02:19:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-connections/m-p/446977#M26417</guid>
      <dc:creator>thomaskang-b295</dc:creator>
      <dc:date>2015-05-22T02:19:43Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG connections</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-connections/m-p/446978#M26418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Luiz, I use a Segger J-Link with the K22F and K64F which also has a 20pin connector.&amp;nbsp; However, there is a 10pin Cortex-M adapter that plugs into the hardware and then has a 10pin ribbon connection.&amp;nbsp; So you likely really only need these connections.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30810iD01FD63285B7F8A0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2015 15:36:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-connections/m-p/446978#M26418</guid>
      <dc:creator>dave408</dc:creator>
      <dc:date>2015-05-22T15:36:31Z</dc:date>
    </item>
  </channel>
</rss>