<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: TWR-K60N512 how to flash - beginner question</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-how-to-flash-beginner-question/m-p/152397#M263</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;thx for your reply. The flashing process works. I have tested it with the pre-built uTasker binary. E1 is blinking now (as described on your page). The ethernet connection doesn't work - should there be a shell or something like that on the serial port? I have tried to get output from the TWR-SER and the virtual serial interface without success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jumper:&lt;/P&gt;&lt;P&gt;CPU Board&lt;/P&gt;&lt;P&gt;J1 - connected&lt;/P&gt;&lt;P&gt;J2 - not connected&lt;/P&gt;&lt;P&gt;J6 - 2 and 3 connected&lt;/P&gt;&lt;P&gt;J8 - connected&lt;/P&gt;&lt;P&gt;J9 - 2 and 3 connected&lt;/P&gt;&lt;P&gt;J10 - not connected&lt;/P&gt;&lt;P&gt;J12 - connected&lt;/P&gt;&lt;P&gt;J16 - not connected&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;TWR-SER&lt;/P&gt;&lt;P&gt;J2 - 3 and 4 connected&lt;/P&gt;&lt;P&gt;J3 - 2 and 3 connected&lt;/P&gt;&lt;P&gt;J10 - 1 and 2 connected&lt;/P&gt;&lt;P&gt;J12 - 9 and 10 connected&lt;/P&gt;&lt;P&gt;J15 - 1 and 2 connected&lt;/P&gt;&lt;P&gt;J17 - 1 and 2 connected&lt;/P&gt;&lt;P&gt;J19 - 1 and 2 connected&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;flo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Apr 2012 16:50:45 GMT</pubDate>
    <dc:creator>mich1985</dc:creator>
    <dc:date>2012-04-13T16:50:45Z</dc:date>
    <item>
      <title>TWR-K60N512 how to flash - beginner question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-how-to-flash-beginner-question/m-p/152395#M261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;at the moment i try to get familiar with the TWR-K60N512 &amp;amp; the eclipse based CodeWarrior Version. I have installed the necessary drivers as described in&amp;nbsp;TWRK60N512_QuickStartDemoLAB.pdf. If i connect the tower system and try to flash a sample project (helloworld, mqx or fnet as example) the erasing and flashing process seems to be working fine (finished without erros).&lt;/P&gt;&lt;P&gt;After a reset of the tower system there is still the previous running demo application. Is there any jumper or something like that which protects the flash memory to be written?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;flo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2012 14:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-how-to-flash-beginner-question/m-p/152395#M261</guid>
      <dc:creator>mich1985</dc:creator>
      <dc:date>2012-04-09T14:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60N512 how to flash - beginner question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-how-to-flash-beginner-question/m-p/152396#M262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are no jumpers to protect memory.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Check that you are building a target that is located in Flash. It may be that the target that you are testing is loading to RAM, which would mean that it can run (when there is enough RAM available for it) but the original Flash based code is still operating after a reset.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note also that CW10.2 has a Flash utility built in to it while also allows any file on the PC (binary or HEX) to be loaded to Flash. You can get pre-built examples for your board here: &lt;A href="http://www.utasker.com/SW_Demos.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/SW_Demos.html&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Apr 2012 22:33:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-how-to-flash-beginner-question/m-p/152396#M262</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2012-04-09T22:33:54Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60N512 how to flash - beginner question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-how-to-flash-beginner-question/m-p/152397#M263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;thx for your reply. The flashing process works. I have tested it with the pre-built uTasker binary. E1 is blinking now (as described on your page). The ethernet connection doesn't work - should there be a shell or something like that on the serial port? I have tried to get output from the TWR-SER and the virtual serial interface without success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jumper:&lt;/P&gt;&lt;P&gt;CPU Board&lt;/P&gt;&lt;P&gt;J1 - connected&lt;/P&gt;&lt;P&gt;J2 - not connected&lt;/P&gt;&lt;P&gt;J6 - 2 and 3 connected&lt;/P&gt;&lt;P&gt;J8 - connected&lt;/P&gt;&lt;P&gt;J9 - 2 and 3 connected&lt;/P&gt;&lt;P&gt;J10 - not connected&lt;/P&gt;&lt;P&gt;J12 - connected&lt;/P&gt;&lt;P&gt;J16 - not connected&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;TWR-SER&lt;/P&gt;&lt;P&gt;J2 - 3 and 4 connected&lt;/P&gt;&lt;P&gt;J3 - 2 and 3 connected&lt;/P&gt;&lt;P&gt;J10 - 1 and 2 connected&lt;/P&gt;&lt;P&gt;J12 - 9 and 10 connected&lt;/P&gt;&lt;P&gt;J15 - 1 and 2 connected&lt;/P&gt;&lt;P&gt;J17 - 1 and 2 connected&lt;/P&gt;&lt;P&gt;J19 - 1 and 2 connected&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;flo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Apr 2012 16:50:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-how-to-flash-beginner-question/m-p/152397#M263</guid>
      <dc:creator>mich1985</dc:creator>
      <dc:date>2012-04-13T16:50:45Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K60N512 how to flash - beginner question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-how-to-flash-beginner-question/m-p/152398#M264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem solved (changed Jumper 1 - strange...).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2012 22:54:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60N512-how-to-flash-beginner-question/m-p/152398#M264</guid>
      <dc:creator>mich1985</dc:creator>
      <dc:date>2012-04-25T22:54:01Z</dc:date>
    </item>
  </channel>
</rss>