<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Signal graph with eGUI</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Signal-graph-with-eGUI/m-p/443675#M26140</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Elisa,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did the answer from Luis Casado in the thread below answer your question?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/539838"&gt;Re: eGUI 3.0 demo on TWR-LCD-RGB&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jul 2015 15:55:45 GMT</pubDate>
    <dc:creator>EarlOrlando</dc:creator>
    <dc:date>2015-07-29T15:55:45Z</dc:date>
    <item>
      <title>Signal graph with eGUI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Signal-graph-with-eGUI/m-p/443674#M26139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to graph a sinusoidal signal using the graph object from eGUI. I'm using the TWR-LCD-RGB and the TWR-K70 module.&lt;/P&gt;&lt;P&gt;What I'm doing is using the ADC0 and acquiring the sinusoidal from a function generator. I acquire the data and then convert it to float after mapping the acquired data. According to what I've found I need to add data to the traces of the graph, the format of this data being D4D_GRAPH_VALUE, but apparently the D4D_GRAPH_VALUE data type retrieves integers and no float values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What should I do to graph the sinusoidal signal?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Elisa &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2015 15:36:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Signal-graph-with-eGUI/m-p/443674#M26139</guid>
      <dc:creator>elisamejia</dc:creator>
      <dc:date>2015-07-24T15:36:31Z</dc:date>
    </item>
    <item>
      <title>Re: Signal graph with eGUI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Signal-graph-with-eGUI/m-p/443675#M26140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Elisa,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did the answer from Luis Casado in the thread below answer your question?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/539838"&gt;Re: eGUI 3.0 demo on TWR-LCD-RGB&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 15:55:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Signal-graph-with-eGUI/m-p/443675#M26140</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2015-07-29T15:55:45Z</dc:date>
    </item>
  </channel>
</rss>