<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Installizing GPIO input/outputs</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443671#M26136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53547i151CF1E5E5DA7E6A/image-size/large?v=v2&amp;amp;px=999" title="program flow chart.PNG" alt="program flow chart.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Ok so I've made a diagram of how the program/(part of the circuit) will be set out so you can get a much clearer picture on what i need to do sorry for the confusion with the "2 buttons" before.&lt;/P&gt;&lt;P&gt;so if you press the button but haven't pulled out the pull out it will play a noise on loop and when you press it&lt;/P&gt;&lt;P&gt;again it will turn off. But if you have taken the pullout out it puts it into an "ACTIVE" mode so as soon as you press&lt;/P&gt;&lt;P&gt;the button it will start playing and won't stop until the batteries die no matter how many times you try to turn it off.&lt;/P&gt;&lt;P&gt;define: GPIO, noise function, speaker function, &lt;/P&gt;&lt;P&gt;1. A low speed voltage is put through both the GPIO outputs.&lt;/P&gt;&lt;P&gt;2. Both the GPIO inputs keep sampling for any input.&lt;/P&gt;&lt;P&gt;3.Outcomes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; A. The "contact" gets an input and the button does as well it will jump to the part of the code where it will just play the noise on loop&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; until the batteries die.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; B, Their is an input in the button function but not the "contact" functions it will start playing the code that just plays the noise on loop until the button is&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pressed again to turn it off&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 16 Aug 2015 10:02:27 GMT</pubDate>
    <dc:creator>jackmonaghan</dc:creator>
    <dc:date>2015-08-16T10:02:27Z</dc:date>
    <item>
      <title>Installizing GPIO input/outputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443667#M26132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I'm using the Kinetis KL43Z MCU and have 2 question&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. How do I setup a GPIO input and out put function (could you please provide a sample along with explanation)&lt;/P&gt;&lt;P&gt;2. Can you please give me a list of the GPIO names used on this MCU&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is greatly appreciated&lt;/P&gt;&lt;P&gt;Kind regards Jack Monaghan​&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Aug 2015 01:01:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443667#M26132</guid>
      <dc:creator>jackmonaghan</dc:creator>
      <dc:date>2015-08-15T01:01:21Z</dc:date>
    </item>
    <item>
      <title>Re: Installizing GPIO input/outputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443668#M26133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jack&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. See the following for macros to configure and control GPIOs in the uTasker project - the macro source code shows the actual control that they do.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/forum/index.php?topic=1875.0" title="http://www.utasker.com/forum/index.php?topic=1875.0"&gt;Kinetis Port Macros&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Below is a screen shot of the uTasker simulator running the FRDM-KL43Z board. Attached is the simulation (simply unzip and execute uTaskerFRDM-KL43Z - no installation necessary) - if you hover the mouse over each port you can see its pin number, its GPIO and peripheral functions as well as the present function that it has (whether input or output and logical state) - if an interrupt is configured on a port changing its input state by clicking with the mouse will also cause interrupt to be generated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52492i2D2096FEC35FB87D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Otherwise you can find a complete list of pins in the KL43 user manual in the section about pin multiplexing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you would like to accelerate your learing and have much more fun in the process simply use the uTasker project and the KL43 simulator and you can step through the code that controls such things and test you own code - and see the results in the simuator without needing to use a debuger or guess what is happening in the chip.&lt;/P&gt;&lt;P&gt;All tools and code are free for non-commerical work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;KL43: &lt;A href="http://www.utasker.com/kinetis/FRDM-KL43Z.html" title="http://www.utasker.com/kinetis/FRDM-KL43Z.html"&gt;µTasker FRDM-KL43Z support&lt;/A&gt;&amp;nbsp; / &lt;A href="http://www.utasker.com/kinetis/TWR-KL43Z48M.html" title="http://www.utasker.com/kinetis/TWR-KL43Z48M.html"&gt;µTasker TWR-KL43Z48M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Aug 2015 01:41:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443668#M26133</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-08-15T01:41:45Z</dc:date>
    </item>
    <item>
      <title>Re: Installizing GPIO input/outputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443669#M26134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please help me make 2 functions for 2 buttons?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Aug 2015 04:23:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443669#M26134</guid>
      <dc:creator>jackmonaghan</dc:creator>
      <dc:date>2015-08-15T04:23:03Z</dc:date>
    </item>
    <item>
      <title>Re: Installizing GPIO input/outputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443670#M26135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jack&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will need to better specifiy what you require but the following shows how I would configure two inputs to monitor two buttons. One is moitored by polling and one is configured to generate an interrupt when pressed (assuming they are '0' when pressed).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE&gt;#define BUTTON1&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTB_BIT0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // button inputs to use
#define BUTTON2&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTC_BIT3&amp;nbsp; 

void fnConfigureButtons(void) {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTERRUPT_SETUP interrupt_setup;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // interrupt configuration parameters
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup.int_handler = fnButton1_pressed;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // handling function
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup.int_priority = 3;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // port interrupt priority
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup.int_port = PORTB;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // the port used
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup.int_port_sense = (IRQ_FALLING_EDGE | PULLUP_ON);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // interrupt on rising edges
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; interrupt_setup.int_port_bits = (BUTTON1);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // the inputs connected
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnConfigureInterrupt((void *)&amp;amp;interrupt_setup);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // configure interrupt on button 1
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _CONFIG_PORT_INPUT(C, (BUTTON2), PORT_PS_UP_ENABLE);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // configure button 2 input
 }

void fnPollButton2(void) {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (_READ_PORT_MASK(C, BUTTON2) == 0) {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnDebugMsg("Button 2 is pressed\r\n");
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; else {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnDebugMsg("Button 2 is NOT pressed\r\n");
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }
}

// Interrupt handler when button 1 pressed
//
static void fnButton1_pressed(void)
{
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnInterruptMessage(OWN_TASK, BUTTON_EVENT);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // example of generating an event
}&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis.html" rel="nofollow noopener noreferrer" target="_blank"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;KL43: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/FRDM-KL43Z.html" rel="nofollow noopener noreferrer" target="_blank"&gt;µTasker FRDM-KL43Z support&lt;/A&gt;&amp;nbsp; / &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/TWR-KL43Z48M.html" rel="nofollow noopener noreferrer" target="_blank"&gt;µTasker TWR-KL43Z48M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Aug 2015 10:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443670#M26135</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-08-15T10:42:23Z</dc:date>
    </item>
    <item>
      <title>Re: Installizing GPIO input/outputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443671#M26136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53547i151CF1E5E5DA7E6A/image-size/large?v=v2&amp;amp;px=999" title="program flow chart.PNG" alt="program flow chart.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Ok so I've made a diagram of how the program/(part of the circuit) will be set out so you can get a much clearer picture on what i need to do sorry for the confusion with the "2 buttons" before.&lt;/P&gt;&lt;P&gt;so if you press the button but haven't pulled out the pull out it will play a noise on loop and when you press it&lt;/P&gt;&lt;P&gt;again it will turn off. But if you have taken the pullout out it puts it into an "ACTIVE" mode so as soon as you press&lt;/P&gt;&lt;P&gt;the button it will start playing and won't stop until the batteries die no matter how many times you try to turn it off.&lt;/P&gt;&lt;P&gt;define: GPIO, noise function, speaker function, &lt;/P&gt;&lt;P&gt;1. A low speed voltage is put through both the GPIO outputs.&lt;/P&gt;&lt;P&gt;2. Both the GPIO inputs keep sampling for any input.&lt;/P&gt;&lt;P&gt;3.Outcomes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; A. The "contact" gets an input and the button does as well it will jump to the part of the code where it will just play the noise on loop&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; until the batteries die.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; B, Their is an input in the button function but not the "contact" functions it will start playing the code that just plays the noise on loop until the button is&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pressed again to turn it off&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Aug 2015 10:02:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443671#M26136</guid>
      <dc:creator>jackmonaghan</dc:creator>
      <dc:date>2015-08-16T10:02:27Z</dc:date>
    </item>
    <item>
      <title>Re: Installizing GPIO input/outputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443672#M26137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't see the advantage of connecting one pole of the button/contact to a GPIO output - they can probably be connected to 0V and the inputs can connect an internal pull-up and monitor for a '0' to detect when the button is pressed or the contact is closed.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;In your case you just need to configure these two pins as outputs driving 0V (or '1' and invert the input detection).&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The rest of the logic (and what happens when the inputs are detected) is general software and so has nothing to do with the Kinetis GPIOs themselves.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis.html" rel="nofollow"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;KL43: &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/FRDM-KL43Z.html" rel="nofollow"&gt;µTasker FRDM-KL43Z support&lt;/A&gt;&amp;nbsp; / &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.utasker.com/kinetis/TWR-KL43Z48M.html" rel="nofollow"&gt;µTasker TWR-KL43Z48M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Aug 2015 19:23:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443672#M26137</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-08-16T19:23:36Z</dc:date>
    </item>
    <item>
      <title>Re: Installizing GPIO input/outputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443673#M26138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jack Monaghan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Answer your 2 questions:&lt;/P&gt;&lt;P&gt;1.How do I setup a GPIO input and out put function&lt;/P&gt;&lt;P&gt;&amp;nbsp; If you want to control GPIO, you should use these register: SIM_SCGC5, PORTx_PCRn, GPIO register.&lt;/P&gt;&lt;P&gt;&amp;nbsp; SIM_SCGC5 is used to open port clock.&lt;/P&gt;&lt;P&gt;&amp;nbsp; PORTx_PCRn is used to configure the pin as GPIO function, and whether have interrupt , pullup or pulldown,ect.&lt;/P&gt;&lt;P&gt;&amp;nbsp; GPIO, is used to control the pin as output or input, and get the pin input data or set the port output data.&lt;/P&gt;&lt;P&gt;An example to set PTA5 as output high&lt;/P&gt;&lt;P&gt;&amp;nbsp; SIM_SCGC5 |= SIM_SCGC5_PORTA_MASK; // enable pta port clock&lt;/P&gt;&lt;P&gt;&amp;nbsp; PORTA_PCR5 = PORT_PCR_MUX(01); //pta5 as gapio&lt;/P&gt;&lt;P&gt;&amp;nbsp; GPIOA_PDDR = 1&amp;lt;&amp;lt;5;// pta5 output&lt;/P&gt;&lt;P&gt;&amp;nbsp; GPIOA_PDOR= 1&amp;lt;&amp;lt;5;// pta5 output higg&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Input is the same, just congfigure PORTA_PCR5 use interrupt or not, pullup,etc. then clear GPIOA_PDOR bit5 to set pta5 as input.&lt;/P&gt;&lt;P&gt;If you want to use the interrupt, you should enable the global interrupt and the PORTA interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, we have the sample code for the KL43, please download the code from this link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/software/FRDM-KL43Z-SC-BAREMETAL.exe" title="http://cache.freescale.com/files/32bit/software/FRDM-KL43Z-SC-BAREMETAL.exe"&gt;http://cache.freescale.com/files/32bit/software/FRDM-KL43Z-SC-BAREMETAL.exe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2:Can you please give me a list of the GPIO names used on this MCU&lt;/P&gt;&lt;P&gt;&amp;nbsp; You can find the pin name from the reference manual, chapter 10.1 KL43 Signal Multiplexing and Pin Assignments&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2015 02:45:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Installizing-GPIO-input-outputs/m-p/443673#M26138</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-08-17T02:45:42Z</dc:date>
    </item>
  </channel>
</rss>