<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックSD card 4 bit mode</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/443342#M26100</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I'm developing a project where i'm using kinetis K20 microcontroller where I need to improve the SD card speed communication. Now it's working in 1 bit mode.&lt;/P&gt;&lt;P&gt;Did someone use SD card in 4 bit mode? I tried to develop the SDHC.c file using processor expert 10.2 where I selected 4 bit mode, but the SD card speed doesn't increase.&lt;/P&gt;&lt;P&gt;Does someone help me to start this 4 bit mode?&lt;/P&gt;&lt;P&gt;If I want to switch from SDHC mode to SPI mode, how I can do it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Oct 2015 07:23:58 GMT</pubDate>
    <dc:creator>chobin</dc:creator>
    <dc:date>2015-10-08T07:23:58Z</dc:date>
    <item>
      <title>SD card 4 bit mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/443342#M26100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I'm developing a project where i'm using kinetis K20 microcontroller where I need to improve the SD card speed communication. Now it's working in 1 bit mode.&lt;/P&gt;&lt;P&gt;Did someone use SD card in 4 bit mode? I tried to develop the SDHC.c file using processor expert 10.2 where I selected 4 bit mode, but the SD card speed doesn't increase.&lt;/P&gt;&lt;P&gt;Does someone help me to start this 4 bit mode?&lt;/P&gt;&lt;P&gt;If I want to switch from SDHC mode to SPI mode, how I can do it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Oct 2015 07:23:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/443342#M26100</guid>
      <dc:creator>chobin</dc:creator>
      <dc:date>2015-10-08T07:23:58Z</dc:date>
    </item>
    <item>
      <title>Re: SD card 4 bit mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/443343#M26101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chobin,&lt;/P&gt;&lt;P&gt;I'd like to share a project about Fat File System for SD card using SPI for K20.&lt;/P&gt;&lt;P&gt;The link as below.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-100913"&gt;Sd-Card Fat file system Project for Freescale Kinetis.rar&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2015 03:12:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SD-card-4-bit-mode/m-p/443343#M26101</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-10-09T03:12:14Z</dc:date>
    </item>
  </channel>
</rss>