<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックNeed help with k70</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-with-k70/m-p/442783#M26023</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,can anyone please tell me if k70 MCU can deliver 3.3V signal from one pin(I/O pin) and 1.8v signal from another pin(I/O pin) simultaneously?If yes then which register should be access to make the necessary changes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Oct 2015 16:03:32 GMT</pubDate>
    <dc:creator>sudeepaithal</dc:creator>
    <dc:date>2015-10-29T16:03:32Z</dc:date>
    <item>
      <title>Need help with k70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-with-k70/m-p/442783#M26023</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,can anyone please tell me if k70 MCU can deliver 3.3V signal from one pin(I/O pin) and 1.8v signal from another pin(I/O pin) simultaneously?If yes then which register should be access to make the necessary changes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2015 16:03:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-with-k70/m-p/442783#M26023</guid>
      <dc:creator>sudeepaithal</dc:creator>
      <dc:date>2015-10-29T16:03:32Z</dc:date>
    </item>
    <item>
      <title>Re: Need help with k70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-with-k70/m-p/442784#M26024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For K70 has two DAC modules, customer can use one DAC module output 3.3V voltage and another DAC module output 1.8V voltage.&lt;/P&gt;&lt;P&gt;The K70 is single voltage powered, if customer using VDD 3.3V, then customer also could use one GPIO pin output 3.3V voltage and using a DAC module output 1.8V voltage.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jan 2016 08:57:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-with-k70/m-p/442784#M26024</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-01-05T08:57:03Z</dc:date>
    </item>
  </channel>
</rss>