<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Evaluation Board suggestions in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Evaluation-Board-suggestions/m-p/442704#M26012</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Suresh&lt;/P&gt;&lt;P&gt;The Freedom kl05 use 2 electrodes TSI0 in8 and 9&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55992iAEC6E1448F0E5650/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You can use them with the TSI module without the TSS library, or you can use them (I recommend it) with the TSI module and the TSS library, a good example is instaled when you instal the TSS library, normally on this folder&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_TSS_3_1\examples\FRDMKLXX_DEMO\build\cw\FRDMKL05Z_DEMO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also you can use PE to create a project that use the TSI module and the TSS library&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can download the TSS library from here &lt;A href="http://www.freescale.com/products/sensors/touch-sensors/freescale-touch-sensing-software:TSS?tid=vantss"&gt;TSS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And you can check all the information about the Freedom KL05 here&lt;/P&gt;&lt;H1 style="font-size: 24px; color: #627178; font-weight: 400; text-indent: 0px; font-family: arial, sans-serif; font-style: normal; text-align: start;"&gt;&lt;A href="http://www.freescale.com/products/arm-processors/kinetis-cortex-m/l-series/freescale-freedom-development-platform-for-the-kinetis-kl05-and-kl04-mcus:FRDM-KL05Z"&gt;FRDM-KL05Z&lt;/A&gt;&lt;/H1&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this will help you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Sep 2015 16:27:33 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2015-09-14T16:27:33Z</dc:date>
    <item>
      <title>Evaluation Board suggestions</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Evaluation-Board-suggestions/m-p/442703#M26011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Folks, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new to freescale.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was developing HMI application. I was looking for a evaluation board which has touch input (keys) and uses the kinetis Microcontroller. I would like to get acquainted with TSS library and TSI hardware module of KL05. Kindly suggest me suitable evaluation boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I searched for some boards which have touch input interfaced but they use a TSS library and GPIO method to detect the key not the TSI module of the microcontroller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Suresh Jaggal.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Sep 2015 08:40:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Evaluation-Board-suggestions/m-p/442703#M26011</guid>
      <dc:creator>sureshjaggal</dc:creator>
      <dc:date>2015-09-11T08:40:19Z</dc:date>
    </item>
    <item>
      <title>Re: Evaluation Board suggestions</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Evaluation-Board-suggestions/m-p/442704#M26012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Suresh&lt;/P&gt;&lt;P&gt;The Freedom kl05 use 2 electrodes TSI0 in8 and 9&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55992iAEC6E1448F0E5650/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You can use them with the TSI module without the TSS library, or you can use them (I recommend it) with the TSI module and the TSS library, a good example is instaled when you instal the TSS library, normally on this folder&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_TSS_3_1\examples\FRDMKLXX_DEMO\build\cw\FRDMKL05Z_DEMO&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also you can use PE to create a project that use the TSI module and the TSS library&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can download the TSS library from here &lt;A href="http://www.freescale.com/products/sensors/touch-sensors/freescale-touch-sensing-software:TSS?tid=vantss"&gt;TSS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And you can check all the information about the Freedom KL05 here&lt;/P&gt;&lt;H1 style="font-size: 24px; color: #627178; font-weight: 400; text-indent: 0px; font-family: arial, sans-serif; font-style: normal; text-align: start;"&gt;&lt;A href="http://www.freescale.com/products/arm-processors/kinetis-cortex-m/l-series/freescale-freedom-development-platform-for-the-kinetis-kl05-and-kl04-mcus:FRDM-KL05Z"&gt;FRDM-KL05Z&lt;/A&gt;&lt;/H1&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this will help you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Sep 2015 16:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Evaluation-Board-suggestions/m-p/442704#M26012</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-09-14T16:27:33Z</dc:date>
    </item>
  </channel>
</rss>