<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: What does it take to meet the USB timing specification with the MK22FN1M0VLH12?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-it-take-to-meet-the-USB-timing-specification-with-the/m-p/441228#M25864</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A quick look tells me that the MK24FN1M0 is not available in a 64-pin LQFP package which was one of my objectives.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, in order to meet the USB specification, I'd need to add an external crystal. As I understand it, this would preclude using PTA18 and PTA19 for any of the other functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm OK with that if that's the way to go. The first question that comes to ind is: How might that affect any power saving modes? For example, can I turn the external oscillator on/off as needed for USB communications?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have I read this right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Oct 2015 19:44:08 GMT</pubDate>
    <dc:creator>davepfaltzgraff</dc:creator>
    <dc:date>2015-10-07T19:44:08Z</dc:date>
    <item>
      <title>What does it take to meet the USB timing specification with the MK22FN1M0VLH12?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-it-take-to-meet-the-USB-timing-specification-with-the/m-p/441226#M25862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a basic design using the MK22FN512VLH12, based on the FRDM-K22F board, and want to consider using the MK22FN1M0VLH12 as an upgrade path. However, I see that the 1M0 has the note: The MCGFLLCLK does not meet the USB jitter specifications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can this be handled? Does Freescale expect to release a version of the 1M0 in the near future that does?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Oct 2015 18:46:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-it-take-to-meet-the-USB-timing-specification-with-the/m-p/441226#M25862</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2015-10-07T18:46:17Z</dc:date>
    </item>
    <item>
      <title>Re: What does it take to meet the USB timing specification with the MK22FN1M0VLH12?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-it-take-to-meet-the-USB-timing-specification-with-the/m-p/441227#M25863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The note is for the &lt;STRONG&gt;MCGFLLCLK&lt;/STRONG&gt;, but for USB you can of course use the PLL oscillator instead (&lt;STRONG&gt;MCGPLLCLK&lt;/STRONG&gt;). The main difference is that there is no crystal-less USB device feature in the MK22FN1M0 as there is in the MK22FN512, so you need an external crystal/oscillator. If you need such feature (having internal IRC48M oscillator), then the closest device would be the MK24FN1M0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58860iF5FBD4B763D6F3B8/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Oct 2015 19:28:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-it-take-to-meet-the-USB-timing-specification-with-the/m-p/441227#M25863</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-10-07T19:28:14Z</dc:date>
    </item>
    <item>
      <title>Re: What does it take to meet the USB timing specification with the MK22FN1M0VLH12?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-it-take-to-meet-the-USB-timing-specification-with-the/m-p/441228#M25864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A quick look tells me that the MK24FN1M0 is not available in a 64-pin LQFP package which was one of my objectives.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, in order to meet the USB specification, I'd need to add an external crystal. As I understand it, this would preclude using PTA18 and PTA19 for any of the other functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm OK with that if that's the way to go. The first question that comes to ind is: How might that affect any power saving modes? For example, can I turn the external oscillator on/off as needed for USB communications?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have I read this right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Oct 2015 19:44:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-does-it-take-to-meet-the-USB-timing-specification-with-the/m-p/441228#M25864</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2015-10-07T19:44:08Z</dc:date>
    </item>
  </channel>
</rss>