<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: System set up GUI for TSS (TSS_SystemSetup.h). in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-set-up-GUI-for-TSS-TSS-SystemSetup-h/m-p/440991#M25830</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Suresh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The GUI was a tool available on the TSS 2.3 ( I believe) only for the S08 products, this tool never were released for the Kinetis family, so instead of use the GUI you can use processor expert or copy the file from a sample code and update to your application.&lt;/P&gt;&lt;P&gt;I recommend that you check the application note &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4330.pdf?fsrch=1&amp;amp;sr=9&amp;amp;pageNum=1"&gt;AN4330&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This application note is for the kinetis K40 but the TSI module on the kinetis KL family is very similar to the kinetis K family&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Oct 2015 21:20:26 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2015-10-15T21:20:26Z</dc:date>
    <item>
      <title>System set up GUI for TSS (TSS_SystemSetup.h).</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-set-up-GUI-for-TSS-TSS-SystemSetup-h/m-p/440990#M25829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Folks, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was developing a HMI application using the TSS and TSI of the FRDM-KL05Z.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tools used: Coder warrior 10.6.4&lt;/P&gt;&lt;P&gt;TSS Library : TSS 3.1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was referring to the document How to implement a Human machine Interface Using the Touch Sensing Software Library ( AN394 ) . It is mentioned in the document that we can generate TSS_SystemSetup.h using a gui calle System setup GUI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Start --&amp;gt; Programs --&amp;gt;Freescale --&amp;gt;Touch Sensing Software vx.x --&amp;gt; System Setup GUI&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TSS 3.1 is installed successfully and up to date but i dont find any program to generate TSS_SystemSetup.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could somebody help me how to generate this TSS_SystemSetup.h from the GUI .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Suresh Jaggal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Oct 2015 09:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-set-up-GUI-for-TSS-TSS-SystemSetup-h/m-p/440990#M25829</guid>
      <dc:creator>sureshjaggal</dc:creator>
      <dc:date>2015-10-07T09:33:22Z</dc:date>
    </item>
    <item>
      <title>Re: System set up GUI for TSS (TSS_SystemSetup.h).</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-set-up-GUI-for-TSS-TSS-SystemSetup-h/m-p/440991#M25830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Suresh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The GUI was a tool available on the TSS 2.3 ( I believe) only for the S08 products, this tool never were released for the Kinetis family, so instead of use the GUI you can use processor expert or copy the file from a sample code and update to your application.&lt;/P&gt;&lt;P&gt;I recommend that you check the application note &lt;A href="http://cache.freescale.com/files/sensors/doc/app_note/AN4330.pdf?fsrch=1&amp;amp;sr=9&amp;amp;pageNum=1"&gt;AN4330&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This application note is for the kinetis K40 but the TSI module on the kinetis KL family is very similar to the kinetis K family&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Oct 2015 21:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/System-set-up-GUI-for-TSS-TSS-SystemSetup-h/m-p/440991#M25830</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-10-15T21:20:26Z</dc:date>
    </item>
  </channel>
</rss>