<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックIf I'm using a mk66 part how do I wire it for only using one usb port?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/If-I-m-using-a-mk66-part-how-do-I-wire-it-for-only-using-one-usb/m-p/440676#M25787</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The data sheet only mentions not using both ports:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54561i53A2502A7F7807A2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm thinking tie Vreg_IN0 to Vreg_IN1&lt;/P&gt;&lt;P&gt;I would use the USB1 port so I have bus detect. then float USB0_DP and USB0_DM&lt;/P&gt;&lt;P&gt;Vreg_out would have some caps for filtering but otherwise would not be used.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Jul 2015 15:09:27 GMT</pubDate>
    <dc:creator>jeromeronne</dc:creator>
    <dc:date>2015-07-23T15:09:27Z</dc:date>
    <item>
      <title>If I'm using a mk66 part how do I wire it for only using one usb port?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/If-I-m-using-a-mk66-part-how-do-I-wire-it-for-only-using-one-usb/m-p/440676#M25787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The data sheet only mentions not using both ports:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54561i53A2502A7F7807A2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm thinking tie Vreg_IN0 to Vreg_IN1&lt;/P&gt;&lt;P&gt;I would use the USB1 port so I have bus detect. then float USB0_DP and USB0_DM&lt;/P&gt;&lt;P&gt;Vreg_out would have some caps for filtering but otherwise would not be used.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 15:09:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/If-I-m-using-a-mk66-part-how-do-I-wire-it-for-only-using-one-usb/m-p/440676#M25787</guid>
      <dc:creator>jeromeronne</dc:creator>
      <dc:date>2015-07-23T15:09:27Z</dc:date>
    </item>
    <item>
      <title>Re: If I'm using a mk66 part how do I wire it for only using one usb port?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/If-I-m-using-a-mk66-part-how-do-I-wire-it-for-only-using-one-usb/m-p/440677#M25788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a Note at K66 chapter 53 USB Voltage Regulator:&lt;/P&gt;&lt;P&gt;When USB is not used in the application, it is recommended to connect VREGOUT and VREG_INx together and tie to ground&lt;/P&gt;&lt;P&gt;through a 10kΩ resistor. Do not tie directly to ground, as this causes a latch-up risk. For systems where only one of the VREG_INx pins is ever used, it is also recommended to connect the two VREG_INx pins together.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2015 05:49:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/If-I-m-using-a-mk66-part-how-do-I-wire-it-for-only-using-one-usb/m-p/440677#M25788</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-07-24T05:49:01Z</dc:date>
    </item>
    <item>
      <title>Re: If I'm using a mk66 part how do I wire it for only using one usb port?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/If-I-m-using-a-mk66-part-how-do-I-wire-it-for-only-using-one-usb/m-p/440678#M25789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had decided to just tie the two regulator inputs together. It is always good to get verification that design choices are correct!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 14:32:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/If-I-m-using-a-mk66-part-how-do-I-wire-it-for-only-using-one-usb/m-p/440678#M25789</guid>
      <dc:creator>jeromeronne</dc:creator>
      <dc:date>2015-07-28T14:32:44Z</dc:date>
    </item>
  </channel>
</rss>