<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K21 secure storage in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K21-secure-storage/m-p/440662#M25782</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a customer who is using the K21 with the tamper protection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;They are at the point of wanting to use the K21 32 bytes of secure storage.&lt;/P&gt;&lt;P&gt;The data sheet says the minimum Vbat is 1.71V.&amp;nbsp; Is this the minimum to preserve the data in the 32 bytes?&lt;/P&gt;&lt;P&gt;What is the Vbat voltage to guarantee the 32 bytes of secure storage is cleared?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the K21 unpowered except Vbat can a tamper event clear the 32 bytes?&lt;/P&gt;&lt;P&gt;Is the only way to clear the 32 bytes of secure storage to lower Vbat?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Apr 2015 23:01:00 GMT</pubDate>
    <dc:creator>PHXFAE</dc:creator>
    <dc:date>2015-04-23T23:01:00Z</dc:date>
    <item>
      <title>K21 secure storage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K21-secure-storage/m-p/440662#M25782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a customer who is using the K21 with the tamper protection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;They are at the point of wanting to use the K21 32 bytes of secure storage.&lt;/P&gt;&lt;P&gt;The data sheet says the minimum Vbat is 1.71V.&amp;nbsp; Is this the minimum to preserve the data in the 32 bytes?&lt;/P&gt;&lt;P&gt;What is the Vbat voltage to guarantee the 32 bytes of secure storage is cleared?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the K21 unpowered except Vbat can a tamper event clear the 32 bytes?&lt;/P&gt;&lt;P&gt;Is the only way to clear the 32 bytes of secure storage to lower Vbat?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2015 23:01:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K21-secure-storage/m-p/440662#M25782</guid>
      <dc:creator>PHXFAE</dc:creator>
      <dc:date>2015-04-23T23:01:00Z</dc:date>
    </item>
    <item>
      <title>Re: K21 secure storage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K21-secure-storage/m-p/440663#M25783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Alex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VBAT min that you are refering to is the MIN for the RTC battery supply voltage (1.71V), if you go to section 2.2.1 of the datasheet, you will see the MIN voltage to retain the VBAT register file is between 0.8V - 1.5V, any less will be considered as a VBAT power-on reset&amp;nbsp; and it will erase the 32 byte VBAT register file.&lt;/P&gt;&lt;P&gt;The only way to clear the 32 bytes is during VBAT power-on reset, this module is not affected by the other reset types.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;BR /&gt;Regards!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Patricia Teran&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Apr 2015 21:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K21-secure-storage/m-p/440663#M25783</guid>
      <dc:creator>PatriciaTeran</dc:creator>
      <dc:date>2015-04-24T21:37:02Z</dc:date>
    </item>
    <item>
      <title>Re: K21 secure storage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K21-secure-storage/m-p/440664#M25784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where is the correct answer button.&amp;nbsp; I don't see it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Apr 2015 20:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K21-secure-storage/m-p/440664#M25784</guid>
      <dc:creator>PHXFAE</dc:creator>
      <dc:date>2015-04-27T20:29:57Z</dc:date>
    </item>
    <item>
      <title>Re: K21 secure storage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K21-secure-storage/m-p/440665#M25785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You have to Log in, in order to see it. It should be right below the post with the answer, like this&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50006iB821F35FC2A58E70/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2015 20:52:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K21-secure-storage/m-p/440665#M25785</guid>
      <dc:creator>PatriciaTeran</dc:creator>
      <dc:date>2015-04-28T20:52:59Z</dc:date>
    </item>
    <item>
      <title>Re: K21 secure storage</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K21-secure-storage/m-p/440666#M25786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am logged in and there is no button like you show anywhere on the page.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2015 20:59:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K21-secure-storage/m-p/440666#M25786</guid>
      <dc:creator>PHXFAE</dc:creator>
      <dc:date>2015-04-28T20:59:10Z</dc:date>
    </item>
  </channel>
</rss>