<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Programming MK10DN512ZVLL10 to control MC13233</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-MK10DN512ZVLL10-to-control-MC13233/m-p/440660#M25781</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="ES-MX" style="color: #1f497d;"&gt;Hello Niki,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;I ignore why all those communications are used with the MC13233. It is true only one peripheral (UART or IIC) would be necessary to communicate with it, but the final application might use the other ones for any specific purpose. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;In other words, only the UART or IIC, along with the radio-specific signals, would be enough to control and manage wireless transmissions through the MC13233. Nevertheless, it is up to the final application to use as many interfaces as needed. I guess the design you are referring to does more than simply transmitting data over the air. You should double check with the developers. Or simply ignore the rest of connections if you will not use them. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;We do not have specific demos for Kinetis K10 and MC13233 at all. However, you could use any f the MC13233 examples included in BeeKit such as SMAC Wireless UART to interface them. With such application running in MC13233, any data received via UART 8either form a PC or another MCU) will be sent over the air and vice versa. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;AngelC &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Aug 2015 20:29:17 GMT</pubDate>
    <dc:creator>AngelC</dc:creator>
    <dc:date>2015-08-17T20:29:17Z</dc:date>
    <item>
      <title>Programming MK10DN512ZVLL10 to control MC13233</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-MK10DN512ZVLL10-to-control-MC13233/m-p/440659#M25780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;Hello everyone,&lt;/SPAN&gt;&lt;BR /&gt; &lt;SPAN class="hps"&gt;I have&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;a card where&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;there is&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;an&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;integrated&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;MC13233&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;controlled by a&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;micro&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;MK10DN512ZVLL10&lt;/SPAN&gt;. &lt;SPAN class="hps"&gt;As you can&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;see from the&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;figure below&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;are&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;associated&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;with&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;different&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;communication protocols&lt;/SPAN&gt; &lt;SPAN class="hps atn"&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;UART&lt;/SPAN&gt;, &lt;SPAN class="hps"&gt;IIC&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;and&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;TMP&lt;/SPAN&gt;&lt;SPAN&gt;)&lt;/SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54404iE7D480E7CE5F0F06/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;SPAN lang="en"&gt;&lt;BR /&gt; &lt;SPAN class="hps"&gt;I wanted to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;ask&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;all three&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;are&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;really necessary&lt;/SPAN&gt;?&lt;BR /&gt; &lt;SPAN class="hps"&gt;Someone&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;has scheduled&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;a&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;MC13233&lt;/SPAN&gt;? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;You&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;could&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;give you an indication&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;of how to do&lt;/SPAN&gt;&lt;SPAN&gt;?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Aug 2015 15:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-MK10DN512ZVLL10-to-control-MC13233/m-p/440659#M25780</guid>
      <dc:creator>nikivendola</dc:creator>
      <dc:date>2015-08-16T15:48:41Z</dc:date>
    </item>
    <item>
      <title>Re: Programming MK10DN512ZVLL10 to control MC13233</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-MK10DN512ZVLL10-to-control-MC13233/m-p/440660#M25781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="ES-MX" style="color: #1f497d;"&gt;Hello Niki,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;I ignore why all those communications are used with the MC13233. It is true only one peripheral (UART or IIC) would be necessary to communicate with it, but the final application might use the other ones for any specific purpose. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;In other words, only the UART or IIC, along with the radio-specific signals, would be enough to control and manage wireless transmissions through the MC13233. Nevertheless, it is up to the final application to use as many interfaces as needed. I guess the design you are referring to does more than simply transmitting data over the air. You should double check with the developers. Or simply ignore the rest of connections if you will not use them. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;We do not have specific demos for Kinetis K10 and MC13233 at all. However, you could use any f the MC13233 examples included in BeeKit such as SMAC Wireless UART to interface them. With such application running in MC13233, any data received via UART 8either form a PC or another MCU) will be sent over the air and vice versa. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;AngelC &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2015 20:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Programming-MK10DN512ZVLL10-to-control-MC13233/m-p/440660#M25781</guid>
      <dc:creator>AngelC</dc:creator>
      <dc:date>2015-08-17T20:29:17Z</dc:date>
    </item>
  </channel>
</rss>