<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MK20DN128VFM5 - SWD Does not connect - Silicon version inconsistencies</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN128VFM5-SWD-Does-not-connect/m-p/438409#M25626</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi M J,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a FRDM-K20D50M board on hand, which with a K20 50MHz mask set: 1N86B on board.&lt;/P&gt;&lt;P&gt;I can use J-Link with SWD to debug this board.&lt;/P&gt;&lt;P&gt;So, I think the mask set 1N86B is not the root cause.&lt;/P&gt;&lt;P&gt;I would recommend customer to refer &lt;A href="http://cache.freescale.com/files/microcontrollers/hardware_tools/schematics/FRDM-K20D50M_SCH.pdf"&gt;FRDM-K20D50M schematics&lt;/A&gt; about SWD interface design.&lt;/P&gt;&lt;P&gt;And which debugger tool customer is using? Segger J-Link or P&amp;amp;E Multilink Universal?&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IAR debugger setting:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="iar.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37735iE731E2A95C48C0E7/image-size/large?v=v2&amp;amp;px=999" role="button" title="iar.png" alt="iar.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 May 2015 07:21:24 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2015-05-20T07:21:24Z</dc:date>
    <item>
      <title>MK20DN128VFM5 - SWD Does not connect</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN128VFM5-SWD-Does-not-connect/m-p/438408#M25625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi There,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now having problmes getting a custom desing to connect with the MK20DN128VFM5.&amp;nbsp; I finally figured out an unconnecting SWD issue on a previous custom K22F board&amp;nbsp; that I thought I might be having the same issue on - not the case.&amp;nbsp; Previously the problem was the NMI triggering interrupts which would not allow SWD connection (k22f - no longer connects to SWD ) - reference: &lt;A href="https://community.nxp.com/message/508863"&gt;k22f - no longer connects to SWD&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based upon the reference manual section 6.3.4 the only pins that would conflict with the SWD connection process are the NMI/EZ_PORT_CS(PTA4)&amp;nbsp; and the reset pins.&amp;nbsp; However, I have ensured the that PTA4 is held high during the boot process, observed the reset pin coming high after power on and SWD will not connect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN dir="ltr"&gt;I have previously designed a board with a PK20 (pre-qualified 1n86b silicon) chip pcb which have used in the past and based this current design on the working design.&amp;nbsp; &lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN dir="ltr"&gt;I test the MK20 1n86B silicon chip on the previously running custom board and it will not connect to SWD.&amp;nbsp; &lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN dir="ltr"&gt;I test the PK20 1n86B on my new board and it connects to SWD no problem&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN dir="ltr"&gt;I test the MK20 Nn86B on the K22F freedom board (SDA chip location) and it will not connect using SWD.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN dir="ltr"&gt; I pull an Mk20 3n86B (latest silicon version) chip off of a K22F freedom board and test it on my current design and it connects no problems!&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN dir="ltr"&gt;So it appears that the issue is within the MK20 1n86B silicon version of the chip and I cannot find any reason that SWD would not connect based upon all of the information in the silicon errata.&amp;nbsp; Any further ideas to what might be causing this silicon version to not properly boot/ connect to SWD?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;The easy solution would be to get a hold of the latest silicon version MK20 3n86B chips.&amp;nbsp; I just ordered some MK20DN128VFM5 from digikey and I recieved the old 1n86B silicon chips.&amp;nbsp; Is there anyway to order and ensure I receive the latest silicon?&lt;/LI&gt;&lt;/OL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2015 22:01:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN128VFM5-SWD-Does-not-connect/m-p/438408#M25625</guid>
      <dc:creator>mjg8t</dc:creator>
      <dc:date>2015-05-15T22:01:56Z</dc:date>
    </item>
    <item>
      <title>Re: MK20DN128VFM5 - SWD Does not connect - Silicon version inconsistencies</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN128VFM5-SWD-Does-not-connect/m-p/438409#M25626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi M J,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a FRDM-K20D50M board on hand, which with a K20 50MHz mask set: 1N86B on board.&lt;/P&gt;&lt;P&gt;I can use J-Link with SWD to debug this board.&lt;/P&gt;&lt;P&gt;So, I think the mask set 1N86B is not the root cause.&lt;/P&gt;&lt;P&gt;I would recommend customer to refer &lt;A href="http://cache.freescale.com/files/microcontrollers/hardware_tools/schematics/FRDM-K20D50M_SCH.pdf"&gt;FRDM-K20D50M schematics&lt;/A&gt; about SWD interface design.&lt;/P&gt;&lt;P&gt;And which debugger tool customer is using? Segger J-Link or P&amp;amp;E Multilink Universal?&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IAR debugger setting:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="iar.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37735iE731E2A95C48C0E7/image-size/large?v=v2&amp;amp;px=999" role="button" title="iar.png" alt="iar.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 07:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN128VFM5-SWD-Does-not-connect/m-p/438409#M25626</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-05-20T07:21:24Z</dc:date>
    </item>
    <item>
      <title>Re: MK20DN128VFM5 - SWD Does not connect - Silicon version inconsistencies</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN128VFM5-SWD-Does-not-connect/m-p/438410#M25627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ma,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for confirming that you have a 1n86B version running on your fdm-k22F board.&amp;nbsp; I have re-soldered a 1n86B chip onto the freedom board and it is connecting to SWD on my side as well.&amp;nbsp; I have found that our custom footprint could be improved for better soldering repeatability.&amp;nbsp; I have gotten the 1n86B chips working on our custom prototype boards as well after reworking the boards a few times for proper soldering connections.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It appears I led us on a bit of a goose chase based upon some bad soldering from the beginning.&amp;nbsp; I will see if I can re-label the topic to better reflect the problem.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the support!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 17:31:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DN128VFM5-SWD-Does-not-connect/m-p/438410#M25627</guid>
      <dc:creator>mjg8t</dc:creator>
      <dc:date>2015-05-20T17:31:32Z</dc:date>
    </item>
  </channel>
</rss>