<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: flexnvm as eeprom in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexnvm-as-eeprom/m-p/438353#M25622</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello sanjay jadhav:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an application note about using Flex memory in Kinetis devices:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From your comment I assume the board is a FRDM-K20D50M. The MCU on-board is a MK20DX128VLH5. You can download the &lt;STRONG&gt;C90TFS&lt;/STRONG&gt; flash driver from this link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe" title="http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe"&gt;http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then once installed you will find an example for MK20DX128xxx5 in this path:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"...\Standard_Software_Driver_v1.03\C90TFS\Demos\build\MK20DX128xxx5"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Jun 2015 20:21:10 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2015-06-09T20:21:10Z</dc:date>
    <item>
      <title>flexnvm as eeprom</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexnvm-as-eeprom/m-p/438351#M25620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi i am using frdm k20dm128 board i want use flexnvm as eeprom so plz reply if&amp;nbsp; any buddy have source code or any detail.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jun 2015 12:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexnvm-as-eeprom/m-p/438351#M25620</guid>
      <dc:creator>sanjayjadhav77</dc:creator>
      <dc:date>2015-06-08T12:20:13Z</dc:date>
    </item>
    <item>
      <title>Re: flexnvm as eeprom</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexnvm-as-eeprom/m-p/438352#M25621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello sanjay,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please configure Flash register refer to the reference manual -&amp;gt; 28.4.11.14 Program Partition Command&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35347iE69BBBD9833FB06A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2015 03:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexnvm-as-eeprom/m-p/438352#M25621</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-06-09T03:12:01Z</dc:date>
    </item>
    <item>
      <title>Re: flexnvm as eeprom</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexnvm-as-eeprom/m-p/438353#M25622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello sanjay jadhav:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an application note about using Flex memory in Kinetis devices:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4282.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From your comment I assume the board is a FRDM-K20D50M. The MCU on-board is a MK20DX128VLH5. You can download the &lt;STRONG&gt;C90TFS&lt;/STRONG&gt; flash driver from this link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe" title="http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe"&gt;http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then once installed you will find an example for MK20DX128xxx5 in this path:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"...\Standard_Software_Driver_v1.03\C90TFS\Demos\build\MK20DX128xxx5"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2015 20:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexnvm-as-eeprom/m-p/438353#M25622</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-06-09T20:21:10Z</dc:date>
    </item>
  </channel>
</rss>