<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFlexCAN driver for K60 tower board using kDS</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-driver-for-K60-tower-board-using-kDS/m-p/438331#M25612</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;&amp;nbsp; we dont have much knowledge in CAN communication.I study something. now i have to test the communication using KDS.So please tell me any idea&lt;/P&gt;&lt;P&gt;or please give any sample code to test the can communication.in that tower module there 2 can nodes.....&lt;/P&gt;&lt;P&gt;can we test the CAN using one node using loop back how?&lt;/P&gt;&lt;P&gt;how can we transfer CAN packets?&lt;/P&gt;&lt;P&gt;please give me sample code to test the board please&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Sep 2015 07:29:10 GMT</pubDate>
    <dc:creator>lijofrancis</dc:creator>
    <dc:date>2015-09-10T07:29:10Z</dc:date>
    <item>
      <title>FlexCAN driver for K60 tower board using kDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-driver-for-K60-tower-board-using-kDS/m-p/438331#M25612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;&amp;nbsp; we dont have much knowledge in CAN communication.I study something. now i have to test the communication using KDS.So please tell me any idea&lt;/P&gt;&lt;P&gt;or please give any sample code to test the can communication.in that tower module there 2 can nodes.....&lt;/P&gt;&lt;P&gt;can we test the CAN using one node using loop back how?&lt;/P&gt;&lt;P&gt;how can we transfer CAN packets?&lt;/P&gt;&lt;P&gt;please give me sample code to test the board please&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Sep 2015 07:29:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-driver-for-K60-tower-board-using-kDS/m-p/438331#M25612</guid>
      <dc:creator>lijofrancis</dc:creator>
      <dc:date>2015-09-10T07:29:10Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN driver for K60 tower board using kDS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-driver-for-K60-tower-board-using-kDS/m-p/438332#M25613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lijo, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please, have you tried KSDK example for FlexCAN?&lt;/P&gt;&lt;P&gt;FlexCAN example application demonstrates the SDK Peripheral drivers working with different methods.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two provided examples:&lt;/P&gt;&lt;P&gt;• &lt;STRONG&gt;CAN network:&lt;/STRONG&gt; transfers data through the CAN interface. On node 1, the user inputs characters by&lt;/P&gt;&lt;P&gt;using the UART debug terminal and sends the data with the FlexCAN interface. On the other node,&lt;/P&gt;&lt;P&gt;the FlexCAN receives the data and prints it to the UART terminal.&lt;/P&gt;&lt;P&gt;• &lt;STRONG&gt;CAN loop-back&lt;/STRONG&gt;: transfers data through the CAN loop-back interface. On one node, one 8-byte&lt;/P&gt;&lt;P&gt;buffer stream transmitter output is internally sent back to the receiver input.&lt;/P&gt;&lt;P&gt;The board transfers and receives characters through the FlexCAN-UART interface. Type the characters&lt;/P&gt;&lt;P&gt;on the keyboard and the board receives and displays them on the terminal screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Sep 2015 11:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCAN-driver-for-K60-tower-board-using-kDS/m-p/438332#M25613</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2015-09-10T11:21:56Z</dc:date>
    </item>
  </channel>
</rss>