<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: GCC Linker script for FSL Bootloader</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437798#M25582</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tipoftheswrd,&lt;/P&gt;&lt;P&gt;I'd like to suggest that you can disable the SystemInit() function in the application project at first, then program the compiled binary to the MCU and check whether the MCU can work fine or not.&lt;/P&gt;&lt;P&gt;I'm looking forward to the testing result.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jul 2015 08:26:41 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2015-07-02T08:26:41Z</dc:date>
    <item>
      <title>GCC Linker script for FSL Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437792#M25576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently working on the FSL_Kinetis_Bootloader 1.1.0 and I'd like to use it in combination with my GCC compiled binary.&lt;/P&gt;&lt;P&gt;The flashing through the HID device and the supplied KinetusUpdater.exe works fine (albeit a little slow).&lt;/P&gt;&lt;P&gt;However since I'm using GCC the linker scripts for my application is quite different then IAR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My memory regions are layed at to start the user application at address 0x8000 but this causes a HardFault.&lt;/P&gt;&lt;P&gt;However, it is my user application's HardFault handler so I know flashing has succeeded.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;MEMORY&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;{&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp; VECTORS (rx) : ORIGIN = 0x00008000, LENGTH = 0x00000400&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp; FLASH_PROTECTION&amp;nbsp;&amp;nbsp;&amp;nbsp; (rx) : ORIGIN = 0x00008400, LENGTH = 0x00000010&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp; FLASH (rx) : ORIGIN = 0x00008410, LENGTH = 128K - 0x00008410&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp; RAM (rwx) : ORIGIN = 0x1FFFF0C0, LENGTH = 16K - 0xC0&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;}&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P&gt;I guess it has something to do with the Bootloader Configuration Area (BCA) but I can't seem to get any useful info from the supplied linker scripts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Jun 2015 07:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437792#M25576</guid>
      <dc:creator>tipofthesowrd</dc:creator>
      <dc:date>2015-06-28T07:55:26Z</dc:date>
    </item>
    <item>
      <title>Re: GCC Linker script for FSL Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437793#M25577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've made very little progress these last few days with this issue.&lt;/P&gt;&lt;P&gt;My guess is the startup code of my user program is not as it should be.&lt;/P&gt;&lt;P&gt;If I look in the led_demo example the IAR startup code has references to the Bootloader configuration area&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, there is no example for a user program with GNU GCC startup code?&lt;/P&gt;&lt;P&gt;Can somebody help adjusting the default GNU GCC startup code to include this Bootloader configuration area?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 07:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437793#M25577</guid>
      <dc:creator>tipofthesowrd</dc:creator>
      <dc:date>2015-06-30T07:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: GCC Linker script for FSL Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437794#M25578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tipoftheswrd,&lt;/P&gt;&lt;P&gt;I'd like to check with you about which MCU you use.&lt;/P&gt;&lt;P&gt;If it's Ok, you can share your application project, then I can reproduce your phenomenon on my board.&lt;/P&gt;&lt;P&gt;I'm looking forward to your reply.&lt;/P&gt;&lt;P&gt;Have a great day!&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 08:59:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437794#M25578</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-06-30T08:59:24Z</dc:date>
    </item>
    <item>
      <title>Re: GCC Linker script for FSL Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437795#M25579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Hi Tipoftheswrd,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;&amp;nbsp; Have you ever tried your application directly without FSL bootloader? Is it running properly?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;&amp;nbsp; BCA will not affect your application if you doesn't have a valid one in it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt; PS: The first member of BCA is tag: 'kcfg', If FSL bootloader fails to check the valid tag then it will use default BCA.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Jay&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 02:01:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437795#M25579</guid>
      <dc:creator>jay_heng</dc:creator>
      <dc:date>2015-07-02T02:01:57Z</dc:date>
    </item>
    <item>
      <title>Re: GCC Linker script for FSL Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437796#M25580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, my original application runs fine if I use the default linker script.&lt;/P&gt;&lt;P&gt;Does the startup code of the user program have to change? Because thes user program will run SystemInit() again to set clocks etc.&lt;/P&gt;&lt;P&gt;Thanks for the information about the BCA tag. This means its probably something simple in my linker script right?&lt;/P&gt;&lt;P&gt;Below is what I currently use for my user program. I'll try and add the binaries later today so Ping can check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;MEMORY&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;{&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp; VECTORS (rx) : ORIGIN = 0x00008000, LENGTH = 0x00000400&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp; FLASH_PROTECTION&amp;nbsp;&amp;nbsp;&amp;nbsp; (rx) : ORIGIN = 0x00008400, LENGTH = 0x00000010&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp; FLASH (rx) : ORIGIN = 0x00008410, LENGTH = 128K - 0x00008410&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp; RAM (rwx) : ORIGIN = 0x1FFFF0C0, LENGTH = 16K - 0xC0&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;}&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Regards&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 06:36:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437796#M25580</guid>
      <dc:creator>tipofthesowrd</dc:creator>
      <dc:date>2015-07-02T06:36:22Z</dc:date>
    </item>
    <item>
      <title>Re: GCC Linker script for FSL Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437797#M25581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi kevin,&lt;/P&gt;&lt;P&gt; I don't think there is any source code change needed for user app, The only thing is to modify the linker file.&lt;/P&gt;&lt;P&gt; Seems your linker file is ok if FSL bootloader specifies the app base address to 0x8000, From the RAM section you defined, seems you wants to copy vector to ram right? you may need to debug into your app to locate the place where the hardfault happens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 08:05:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437797#M25581</guid>
      <dc:creator>jay_heng</dc:creator>
      <dc:date>2015-07-02T08:05:36Z</dc:date>
    </item>
    <item>
      <title>Re: GCC Linker script for FSL Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437798#M25582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tipoftheswrd,&lt;/P&gt;&lt;P&gt;I'd like to suggest that you can disable the SystemInit() function in the application project at first, then program the compiled binary to the MCU and check whether the MCU can work fine or not.&lt;/P&gt;&lt;P&gt;I'm looking forward to the testing result.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 08:26:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437798#M25582</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-07-02T08:26:41Z</dc:date>
    </item>
    <item>
      <title>Re: GCC Linker script for FSL Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437799#M25583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was able to fix the problem. My CMSIS implementation was hard copying the interrupt table from 0x0000 to RAM instad of looking at the SCB-&amp;gt;VTOR register.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2015 08:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GCC-Linker-script-for-FSL-Bootloader/m-p/437799#M25583</guid>
      <dc:creator>tipofthesowrd</dc:creator>
      <dc:date>2015-07-06T08:37:15Z</dc:date>
    </item>
  </channel>
</rss>