<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K22 Flexbus in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436725#M25450</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;I am designing with the K22FX512AVLQ12 in mind.&amp;nbsp; I have a memory interface I put together based on what I understood of the FLEXBUS in the K22P144M120SFV2RM.pdf reference manual.&amp;nbsp; However I have seen several comments in Freescales community boards about problems people are having using a x16 bit data bus.&amp;nbsp; AN4393 doesn't talk about using a non-multiplexed interface for a x16 bit data bus.&amp;nbsp; So, before I make a board, I wanted someone to advise me that this design will work, and if there are other limitations with it if it does.&amp;nbsp; For example, can it read/write an odd or even byte without affecting the corresponding even or odd byte?&amp;nbsp; Will a 32-bit aligned read or write actually result in two memory cycles to the SRAM? Will non-aligned reads and writes work?&amp;nbsp; If the design does work, it should be added to AN4393.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Also, Table-4-1 of the reference manual shows the FLEXBUS to be in 5 different regions of the memory map.&amp;nbsp; The comments I have seen recommend using the "External Peripheral" space.&amp;nbsp; "write-back" and "write-through" suggests a cache, but there is no mention of a cache for the FLEXBUS in the reference manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jul 2015 19:08:37 GMT</pubDate>
    <dc:creator>adamkiburz</dc:creator>
    <dc:date>2015-07-22T19:08:37Z</dc:date>
    <item>
      <title>K22 Flexbus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436725#M25450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;I am designing with the K22FX512AVLQ12 in mind.&amp;nbsp; I have a memory interface I put together based on what I understood of the FLEXBUS in the K22P144M120SFV2RM.pdf reference manual.&amp;nbsp; However I have seen several comments in Freescales community boards about problems people are having using a x16 bit data bus.&amp;nbsp; AN4393 doesn't talk about using a non-multiplexed interface for a x16 bit data bus.&amp;nbsp; So, before I make a board, I wanted someone to advise me that this design will work, and if there are other limitations with it if it does.&amp;nbsp; For example, can it read/write an odd or even byte without affecting the corresponding even or odd byte?&amp;nbsp; Will a 32-bit aligned read or write actually result in two memory cycles to the SRAM? Will non-aligned reads and writes work?&amp;nbsp; If the design does work, it should be added to AN4393.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;Also, Table-4-1 of the reference manual shows the FLEXBUS to be in 5 different regions of the memory map.&amp;nbsp; The comments I have seen recommend using the "External Peripheral" space.&amp;nbsp; "write-back" and "write-through" suggests a cache, but there is no mention of a cache for the FLEXBUS in the reference manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2015 19:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436725#M25450</guid>
      <dc:creator>adamkiburz</dc:creator>
      <dc:date>2015-07-22T19:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: K22 Flexbus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436726#M25451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There should without problem for customer to use 16-bit data port with non-multiplexed mode.&lt;/P&gt;&lt;P&gt;When using the non-multiplexed mode, customer need to make sure the Flexbus pin resource is enough for the application.&lt;/P&gt;&lt;P&gt;For using 16-bit data port, the FB_AD0 pin is obsoleted as address pin, it just read the data with 16 bits (2 bytes).&lt;/P&gt;&lt;P&gt;If there exists address non-aligned, there still could read data out, while it will take more cycles (time).&lt;/P&gt;&lt;P&gt;It could read the odd byte and even byte with byte enable signal.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 03:18:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436726#M25451</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-07-23T03:18:02Z</dc:date>
    </item>
    <item>
      <title>Re: K22 Flexbus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436727#M25452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ma,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for the quick response!&amp;nbsp; I will let you know if I have more questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again.&lt;/P&gt;&lt;P&gt;Adam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 14:17:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436727#M25452</guid>
      <dc:creator>adamkiburz</dc:creator>
      <dc:date>2015-07-23T14:17:34Z</dc:date>
    </item>
    <item>
      <title>Re: K22 Flexbus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436728#M25453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Adam posted this question for me.&amp;nbsp; Please refer to &lt;A href="https://community.nxp.com/thread/364273"&gt;External SRAM and non-multiplexed Flexbus&lt;/A&gt; and comment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mike Huslig&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2015 20:02:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436728#M25453</guid>
      <dc:creator>michaelhuslig</dc:creator>
      <dc:date>2015-08-04T20:02:54Z</dc:date>
    </item>
    <item>
      <title>Re: K22 Flexbus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436729#M25454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ma,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please take a look at the attached schematic and let me know if your answer is still valid?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Adam&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54460i149D68345E171FD6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Aug 2015 22:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436729#M25454</guid>
      <dc:creator>adamkiburz</dc:creator>
      <dc:date>2015-08-04T22:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: K22 Flexbus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436730#M25455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I think customer using FB_AD1 connects with SRAM's A0 is quite right.&lt;/P&gt;&lt;P&gt;Customer need to config Flexbus port size to 16-bit.&lt;/P&gt;&lt;P&gt;For the Kinetis Flexbus module is original from ColdFire product, I attached a ColdFire product MCF54451 Flexbus connects with NOR Flash (16-bit data port) for your reference:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54775i0C7DAB459CE95EC7/image-size/large?v=v2&amp;amp;px=999" title="FlexBUS.png" alt="FlexBUS.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2015 03:11:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Flexbus/m-p/436730#M25455</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-08-05T03:11:34Z</dc:date>
    </item>
  </channel>
</rss>