<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Not able to program the K61</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Not-able-to-program-the-K61/m-p/435943#M25370</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made a schematic with micro controller of MK611FN1M0vM.Im not able to program the micro controller using JTAG.The Error was"No core was found".I checked all the powers and GND,They are properly connected.Even the RESET is also pulled high.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I observed that The RESET_b and JTAG_TRST_b are shorted together and connected to JTAG connector PIN10. &lt;/P&gt;&lt;P&gt;Could you please help me this short of pins may cause the problem of not able to program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Subba.Mudi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 May 2015 09:23:10 GMT</pubDate>
    <dc:creator>subba</dc:creator>
    <dc:date>2015-05-15T09:23:10Z</dc:date>
    <item>
      <title>Not able to program the K61</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Not-able-to-program-the-K61/m-p/435943#M25370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made a schematic with micro controller of MK611FN1M0vM.Im not able to program the micro controller using JTAG.The Error was"No core was found".I checked all the powers and GND,They are properly connected.Even the RESET is also pulled high.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I observed that The RESET_b and JTAG_TRST_b are shorted together and connected to JTAG connector PIN10. &lt;/P&gt;&lt;P&gt;Could you please help me this short of pins may cause the problem of not able to program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Subba.Mudi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2015 09:23:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Not-able-to-program-the-K61/m-p/435943#M25370</guid>
      <dc:creator>subba</dc:creator>
      <dc:date>2015-05-15T09:23:10Z</dc:date>
    </item>
    <item>
      <title>Re: Not able to program the K61</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Not-able-to-program-the-K61/m-p/435944#M25371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would recommend customer to refer &lt;A href="http://cache.freescale.com/files/32bit/hardware_tools/schematics/TWR-K60F120M-SCH_C.pdf"&gt;TWR-K60F120M&lt;/A&gt; board about JTAG debugger interface circuit design.&lt;/P&gt;&lt;P&gt;And there also with &lt;A href="http://cache.freescale.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf"&gt;Kinetis Peripheral Module Quick Reference&lt;/A&gt;, the chapter 2.1.5.3 Debug interface also could help.&lt;/P&gt;&lt;P&gt;While, customer also need to check K61 PTA4 pin, which default function is /EZP_CS.&lt;/P&gt;&lt;P&gt;When this pin with low voltage will enter EzPort mode after reset. Please keep this pin with high voltage during chip power up.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2015 07:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Not-able-to-program-the-K61/m-p/435944#M25371</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-05-18T07:17:57Z</dc:date>
    </item>
  </channel>
</rss>