<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Reset held asserted at first power-up -- K20 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reset-held-asserted-at-first-power-up-K20/m-p/435939#M25368</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've designed a PCB that uses the MK20DX256VLH7.&amp;nbsp; Upon first power-up, the microcontroller appears dead.&amp;nbsp; No 16MHz XTAL oscillation, and the DX256's RESET pin is held asserted.&amp;nbsp; Supply voltage is steady at +3.3V.&amp;nbsp;&amp;nbsp; AT this stage, I've not attached any other devices to the DX256, other than a USB connector.&lt;/P&gt;&lt;P&gt;What issues could be causing the part to be stalled like this?&amp;nbsp;&amp;nbsp; I'm very perplexed at this point. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks, in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jul 2015 17:24:25 GMT</pubDate>
    <dc:creator>garyk_</dc:creator>
    <dc:date>2015-07-22T17:24:25Z</dc:date>
    <item>
      <title>Reset held asserted at first power-up -- K20</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reset-held-asserted-at-first-power-up-K20/m-p/435939#M25368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've designed a PCB that uses the MK20DX256VLH7.&amp;nbsp; Upon first power-up, the microcontroller appears dead.&amp;nbsp; No 16MHz XTAL oscillation, and the DX256's RESET pin is held asserted.&amp;nbsp; Supply voltage is steady at +3.3V.&amp;nbsp;&amp;nbsp; AT this stage, I've not attached any other devices to the DX256, other than a USB connector.&lt;/P&gt;&lt;P&gt;What issues could be causing the part to be stalled like this?&amp;nbsp;&amp;nbsp; I'm very perplexed at this point. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks, in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2015 17:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reset-held-asserted-at-first-power-up-K20/m-p/435939#M25368</guid>
      <dc:creator>garyk_</dc:creator>
      <dc:date>2015-07-22T17:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: Reset held asserted at first power-up -- K20</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reset-held-asserted-at-first-power-up-K20/m-p/435940#M25369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary Kitten,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Actually, to a new chip without program, your phenomena is normal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 16MHZ external oscillator is not oscillating, it is because you didn't enable the OSC in the chip with program.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; To a new chip, if you add 4.7K to 10k pullup resistor in the RESET_b pin, and connect a 100nf capacitor to ground, the reset pin should have&amp;nbsp; the oscillator wave, you can check it through the oscilloscope.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; You can create a sample project, to check whether your chip can download program.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; After the chip have programed, it will work normally.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 02:38:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reset-held-asserted-at-first-power-up-K20/m-p/435940#M25369</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-07-23T02:38:17Z</dc:date>
    </item>
  </channel>
</rss>