<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Routing through NC or unused MAPBGA pins</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Routing-through-NC-or-unused-MAPBGA-pins/m-p/435214#M25319</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That is very helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However can I ask you to confirm that I can route through NC pads because I have since found this thread which seems to disagree: &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/378503"&gt;NC pins on Kinetis K20 based MK20FN1M0VMD12 quick easy question&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Nov 2015 04:01:45 GMT</pubDate>
    <dc:creator>malder</dc:creator>
    <dc:date>2015-11-24T04:01:45Z</dc:date>
    <item>
      <title>Routing through NC or unused MAPBGA pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Routing-through-NC-or-unused-MAPBGA-pins/m-p/435212#M25317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The 121 pin MAPBGA package (MK22FN256) has several 'NC' pins on the periphery of the package. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Routing would be made much easier if we could either route through these pads or not populate the pads at all. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are either of these options possible?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 00:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Routing-through-NC-or-unused-MAPBGA-pins/m-p/435212#M25317</guid>
      <dc:creator>malder</dc:creator>
      <dc:date>2015-11-24T00:29:04Z</dc:date>
    </item>
    <item>
      <title>Re: Routing through NC or unused MAPBGA pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Routing-through-NC-or-unused-MAPBGA-pins/m-p/435213#M25318</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Matt&lt;/P&gt;&lt;P&gt;For NC pins. you can route through when you layout. For pins which have function but no used, you cannot route through.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 02:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Routing-through-NC-or-unused-MAPBGA-pins/m-p/435213#M25318</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2015-11-24T02:52:18Z</dc:date>
    </item>
    <item>
      <title>Re: Routing through NC or unused MAPBGA pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Routing-through-NC-or-unused-MAPBGA-pins/m-p/435214#M25319</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That is very helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However can I ask you to confirm that I can route through NC pads because I have since found this thread which seems to disagree: &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/378503"&gt;NC pins on Kinetis K20 based MK20FN1M0VMD12 quick easy question&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 04:01:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Routing-through-NC-or-unused-MAPBGA-pins/m-p/435214#M25319</guid>
      <dc:creator>malder</dc:creator>
      <dc:date>2015-11-24T04:01:45Z</dc:date>
    </item>
    <item>
      <title>Re: Routing through NC or unused MAPBGA pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Routing-through-NC-or-unused-MAPBGA-pins/m-p/435215#M25320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;At my blog there are links to books on PCB layout including BGA routing: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://blog.softwaresafety.net/2010/03/survival-is-not-mandatory-right-first.html" rel="nofollow"&gt;http://blog.softwaresafety.net/2010/03/survival-is-not-mandatory-right-first.html&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 12:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Routing-through-NC-or-unused-MAPBGA-pins/m-p/435215#M25320</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2015-11-24T12:56:13Z</dc:date>
    </item>
    <item>
      <title>Re: Routing through NC or unused MAPBGA pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Routing-through-NC-or-unused-MAPBGA-pins/m-p/435216#M25321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe I wasn't very clear...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found this thread which suggests that 'NC' pins on the MK20 parts are used for internal testing, and so should not be connected to anything on the board.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/378503"&gt;NC pins on Kinetis K20 based MK20FN1M0VMD12 quick easy question&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the answer in that thread sounds very generic. So I am looking for confirmation. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the MK22FN256 part and there are several NC pins on the periphery. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are these pins connected internally?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not, then I can route through them and it makes life much easier. &lt;/P&gt;&lt;P&gt;If they are used for testing etc then of course I will need to avoid them.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Nov 2015 05:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Routing-through-NC-or-unused-MAPBGA-pins/m-p/435216#M25321</guid>
      <dc:creator>malder</dc:creator>
      <dc:date>2015-11-25T05:07:03Z</dc:date>
    </item>
  </channel>
</rss>