<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Lower baud rate required</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Lower-baud-rate-required/m-p/433659#M25175</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a k10, with a core clock of 92Mhz, and using Uart0, which runs off the core clock. The lowest baud rate I can generate is ( 92,000,000 / 16 ) / SBR. SBR max is 8191, so the lowest baud rate supported is approx 700baud.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Without resorting to changing the core clock frequency, is there any way to make this lower? Some other hidden away divider somewhere perhaps? I don't have the option to change the clock, and want to avoid having to bit bang things.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to get it down to 300baud.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for any help.&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Aug 2015 15:45:42 GMT</pubDate>
    <dc:creator>billnd</dc:creator>
    <dc:date>2015-08-11T15:45:42Z</dc:date>
    <item>
      <title>Lower baud rate required</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Lower-baud-rate-required/m-p/433659#M25175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a k10, with a core clock of 92Mhz, and using Uart0, which runs off the core clock. The lowest baud rate I can generate is ( 92,000,000 / 16 ) / SBR. SBR max is 8191, so the lowest baud rate supported is approx 700baud.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Without resorting to changing the core clock frequency, is there any way to make this lower? Some other hidden away divider somewhere perhaps? I don't have the option to change the clock, and want to avoid having to bit bang things.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to get it down to 300baud.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for any help.&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 15:45:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Lower-baud-rate-required/m-p/433659#M25175</guid>
      <dc:creator>billnd</dc:creator>
      <dc:date>2015-08-11T15:45:42Z</dc:date>
    </item>
    <item>
      <title>Re: Lower baud rate required</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Lower-baud-rate-required/m-p/433660#M25176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello billnd:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately there are no extra dividers. You do not mention the K10 full part number, but depending on the part you could use a UART clocked by the bus clock and get the baudrate down to 350, since the bus is typically configured for half the core clock.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 16:28:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Lower-baud-rate-required/m-p/433660#M25176</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-08-12T16:28:28Z</dc:date>
    </item>
  </channel>
</rss>