<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK60 UART4 with DMA have problems</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-UART4-with-DMA-have-problems/m-p/432906#M25140</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the uart4/Dma to do the serial communication .&lt;/P&gt;&lt;P&gt;The parameters are&lt;/P&gt;&lt;P&gt; BPS: 9600&lt;/P&gt;&lt;P&gt; Parity: Even&lt;/P&gt;&lt;P&gt; Data bits: 7&lt;/P&gt;&lt;P&gt; Stop bits: 2&lt;/P&gt;&lt;P&gt; Flow control: None&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And now I have a problem that&amp;nbsp; I can't set the Stopbits 2. It seems that K60 just&amp;nbsp; support stopbits1 setting.&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 04 Oct 2015 03:31:27 GMT</pubDate>
    <dc:creator>charliezx</dc:creator>
    <dc:date>2015-10-04T03:31:27Z</dc:date>
    <item>
      <title>K60 UART4 with DMA have problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-UART4-with-DMA-have-problems/m-p/432906#M25140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the uart4/Dma to do the serial communication .&lt;/P&gt;&lt;P&gt;The parameters are&lt;/P&gt;&lt;P&gt; BPS: 9600&lt;/P&gt;&lt;P&gt; Parity: Even&lt;/P&gt;&lt;P&gt; Data bits: 7&lt;/P&gt;&lt;P&gt; Stop bits: 2&lt;/P&gt;&lt;P&gt; Flow control: None&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And now I have a problem that&amp;nbsp; I can't set the Stopbits 2. It seems that K60 just&amp;nbsp; support stopbits1 setting.&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Oct 2015 03:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-UART4-with-DMA-have-problems/m-p/432906#M25140</guid>
      <dc:creator>charliezx</dc:creator>
      <dc:date>2015-10-04T03:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: K60 UART4 with DMA have problems</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-UART4-with-DMA-have-problems/m-p/432907#M25141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello charlie zx:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are correct, unfortunately the K60 does not support 2 stop bits.&lt;/P&gt;&lt;P&gt;However you can see the recommendations in the next discussions in the community:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/455343"&gt;K20 UART with 2 stop bit or parity&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/479631"&gt;How can I do 2 stop bits on a K60 UART2 at 9600 baud rate&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Notice however that there is no workaround with DMA.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Oct 2015 04:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-UART4-with-DMA-have-problems/m-p/432907#M25141</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-10-07T04:23:31Z</dc:date>
    </item>
  </channel>
</rss>