<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: regarding MII and RMII interface in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/regarding-MII-and-RMII-interface/m-p/432533#M25089</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no problem to keep MII pin connected (customer can set MII related pin with another function or keep the default setting at Pin Control Register n (PORTx_PCRn) register [MUX] bits).&lt;/P&gt;&lt;P&gt;The RMII operates at 50 MHz and requires synchronization between the PHY and the ENET RMII interface clock input(EXTAL).&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jul 2015 06:13:22 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2015-07-02T06:13:22Z</dc:date>
    <item>
      <title>regarding MII and RMII interface</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/regarding-MII-and-RMII-interface/m-p/432532#M25088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HI everyone&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using freescale K70 series microcontroller (part number MK70FN1M0VMJ12) I have interfaced Ethernet switch IC ( part number LAN9303i) in MII. Whether Can I use this physical  interface in RMII mode by keeping MII pins remain connected or I need to make NC( not connected ). Please confirm on this&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Awaiting your reply&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shiva kumar L V&lt;/P&gt;&lt;P&gt;Hardware Design Engineer - EE Excellence center,&lt;/P&gt;&lt;P&gt;Dover -IIC,&lt;/P&gt;&lt;P&gt;Web site:www.dovercorporation.com&lt;/P&gt;&lt;P&gt;Bangalore&lt;/P&gt;&lt;P&gt;Ph :-8050138478,&lt;/P&gt;&lt;P&gt;Skype ID :- shivakumarlv25@gmail.com&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2015 08:20:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/regarding-MII-and-RMII-interface/m-p/432532#M25088</guid>
      <dc:creator>shivakumarlv</dc:creator>
      <dc:date>2015-05-14T08:20:40Z</dc:date>
    </item>
    <item>
      <title>Re: regarding MII and RMII interface</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/regarding-MII-and-RMII-interface/m-p/432533#M25089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no problem to keep MII pin connected (customer can set MII related pin with another function or keep the default setting at Pin Control Register n (PORTx_PCRn) register [MUX] bits).&lt;/P&gt;&lt;P&gt;The RMII operates at 50 MHz and requires synchronization between the PHY and the ENET RMII interface clock input(EXTAL).&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 06:13:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/regarding-MII-and-RMII-interface/m-p/432533#M25089</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-07-02T06:13:22Z</dc:date>
    </item>
  </channel>
</rss>