<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: how application got valid in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/how-application-got-valid/m-p/432103#M25076</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mahammad Sathalya:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The application entry point or jump address is taken from the application's vector table at the application offset (e.g. for KL25 the offset is 0x8000 by default). Then the jump address is validated as next:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52308i817BF1CD5895105C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Jul 2015 02:43:33 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2015-07-23T02:43:33Z</dc:date>
    <item>
      <title>how application got valid</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/how-application-got-valid/m-p/432102#M25075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Guys , Does any one know , how the bootloader consider is the application is valid or not.. in Kinetis Bootloader code, I am using FRDM kl25z board...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2015 07:24:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/how-application-got-valid/m-p/432102#M25075</guid>
      <dc:creator>mohammads0019</dc:creator>
      <dc:date>2015-07-22T07:24:39Z</dc:date>
    </item>
    <item>
      <title>Re: how application got valid</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/how-application-got-valid/m-p/432103#M25076</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mahammad Sathalya:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The application entry point or jump address is taken from the application's vector table at the application offset (e.g. for KL25 the offset is 0x8000 by default). Then the jump address is validated as next:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52308i817BF1CD5895105C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 02:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/how-application-got-valid/m-p/432103#M25076</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-07-23T02:43:33Z</dc:date>
    </item>
  </channel>
</rss>