<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: I am using freescale K70 series microcontroller (part number MK70FN1M0VMJ12) I have interfaced Ethernet switch IC ( part number LAN9303i) in MII. Whether Can I use this physical  interface in RMII mode by keeping MII pins remain connected or</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-am-using-freescale-K70-series-microcontroller-part-number/m-p/431734#M25057</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that's Ok for customer to connects MII pins with Ethernet PHY, while customer just want to use RMII mode.&lt;/P&gt;&lt;P&gt;Customer could refer &lt;A href="http://cache.freescale.com/files/microcontrollers/hardware_tools/schematics/SCH-26185.pdf"&gt;TWR-SER2&lt;/A&gt; board, which is using DP83849I(two Ethernet PHY) provides MII and RMII connection.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 May 2015 07:06:31 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2015-05-18T07:06:31Z</dc:date>
    <item>
      <title>I am using freescale K70 series microcontroller (part number MK70FN1M0VMJ12) I have interfaced Ethernet switch IC ( part number LAN9303i) in MII. Whether Can I use this physical  interface in RMII mode by keeping MII pins remain connected or</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-am-using-freescale-K70-series-microcontroller-part-number/m-p/431733#M25056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;By&amp;nbsp; keeping&amp;nbsp; physical connection of MII interface can I use RMII mode.or I need to provide jumper settings.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2015 08:23:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-am-using-freescale-K70-series-microcontroller-part-number/m-p/431733#M25056</guid>
      <dc:creator>shivakumarlv</dc:creator>
      <dc:date>2015-05-14T08:23:46Z</dc:date>
    </item>
    <item>
      <title>Re: I am using freescale K70 series microcontroller (part number MK70FN1M0VMJ12) I have interfaced Ethernet switch IC ( part number LAN9303i) in MII. Whether Can I use this physical  interface in RMII mode by keeping MII pins remain connected or</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-am-using-freescale-K70-series-microcontroller-part-number/m-p/431734#M25057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think that's Ok for customer to connects MII pins with Ethernet PHY, while customer just want to use RMII mode.&lt;/P&gt;&lt;P&gt;Customer could refer &lt;A href="http://cache.freescale.com/files/microcontrollers/hardware_tools/schematics/SCH-26185.pdf"&gt;TWR-SER2&lt;/A&gt; board, which is using DP83849I(two Ethernet PHY) provides MII and RMII connection.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2015 07:06:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I-am-using-freescale-K70-series-microcontroller-part-number/m-p/431734#M25057</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-05-18T07:06:31Z</dc:date>
    </item>
  </channel>
</rss>