<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Reset problem with  K02FN128VLH10</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reset-problem-with-K02FN128VLH10/m-p/431534#M25035</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Madam or Sir,&lt;/P&gt;&lt;P&gt;I have hardware problems with the K02FN128VLH10 unfortunately. If I connected the Segger J-link debugger, the application works and the signal Reset has logical 1 level. If I disconnected the debugger and toggle the DC power supply then the application stop running and the Reset pin generate pulses with 10 kHz period approximately. The empty microcontroller generates nothing. I am not sure if it is a hardware or software mistake.&amp;nbsp; I use the standard startup library from the Kinetis studio 2.0 and the developed application works with FRDM-K22F without problem. Really thank you in advance for your help. Your sincerely Michal Pokorny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Apr 2015 06:49:25 GMT</pubDate>
    <dc:creator>michalpokorny</dc:creator>
    <dc:date>2015-04-22T06:49:25Z</dc:date>
    <item>
      <title>Reset problem with  K02FN128VLH10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reset-problem-with-K02FN128VLH10/m-p/431534#M25035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Madam or Sir,&lt;/P&gt;&lt;P&gt;I have hardware problems with the K02FN128VLH10 unfortunately. If I connected the Segger J-link debugger, the application works and the signal Reset has logical 1 level. If I disconnected the debugger and toggle the DC power supply then the application stop running and the Reset pin generate pulses with 10 kHz period approximately. The empty microcontroller generates nothing. I am not sure if it is a hardware or software mistake.&amp;nbsp; I use the standard startup library from the Kinetis studio 2.0 and the developed application works with FRDM-K22F without problem. Really thank you in advance for your help. Your sincerely Michal Pokorny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2015 06:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reset-problem-with-K02FN128VLH10/m-p/431534#M25035</guid>
      <dc:creator>michalpokorny</dc:creator>
      <dc:date>2015-04-22T06:49:25Z</dc:date>
    </item>
    <item>
      <title>Re: Reset problem with  K02FN128VLH10</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reset-problem-with-K02FN128VLH10/m-p/431535#M25036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found your submit the same issue at below thread, please check my feedback at that thread.&lt;/P&gt;&lt;P&gt;Thank you for the understanding.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/353315"&gt;https://community.freescale.com/thread/353315&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Apr 2015 05:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reset-problem-with-K02FN128VLH10/m-p/431535#M25036</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-04-27T05:22:02Z</dc:date>
    </item>
  </channel>
</rss>