<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: PK70FN1M0VMJ12</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK70FN1M0VMJ12/m-p/429387#M24814</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Delpy,&lt;/P&gt;&lt;P&gt;Of course, you need to program the MC9S08JM60 previous, the it can work like a JTAG debug interface to the K70.&lt;/P&gt;&lt;P&gt;You'll learn more information about the OSJTAG through the link as below&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/osbdm/" title="http://www.pemicro.com/osbdm/"&gt;P&amp;amp;E Microcomputer Systems&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 May 2015 02:17:46 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2015-05-06T02:17:46Z</dc:date>
    <item>
      <title>PK70FN1M0VMJ12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK70FN1M0VMJ12/m-p/429384#M24811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wanted to know if the PK70FN1M0VMJ12 can be programmed with other method than JTAG or mini usb please ? because for my project we can program with JTAG only in laboratory&amp;nbsp; and the usb is limited because I don't know if the MC9S08JM60 is sold with a program or not , can you tell me if I can use another method to program the PK70?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MD&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2015 14:34:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK70FN1M0VMJ12/m-p/429384#M24811</guid>
      <dc:creator>delpymatthieu</dc:creator>
      <dc:date>2015-04-21T14:34:35Z</dc:date>
    </item>
    <item>
      <title>Re: PK70FN1M0VMJ12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK70FN1M0VMJ12/m-p/429385#M24812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Delpy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So yes.&amp;nbsp; The PK70 can be programmed with protocols other than JTAG or the USB.&amp;nbsp; You could use Serial Wire Debug (SWD) which is supported by most debug pod vendors (P&amp;amp;E Micro, Segger J-Link, etc,). Using this protocol would require the use of a subset of the JTAG pins (just 2 in fact) and simply a setting change in the software that is driving your debug pod.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alternatively, you could also use the EZport to program your device.&amp;nbsp; For more information on EZport programming, please see chapter 31 in your K70 reference manual.&amp;nbsp; Let us know if one of these methods works for you.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Chris &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2015 15:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK70FN1M0VMJ12/m-p/429385#M24812</guid>
      <dc:creator>chris_brown</dc:creator>
      <dc:date>2015-04-21T15:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: PK70FN1M0VMJ12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK70FN1M0VMJ12/m-p/429386#M24813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank christopher ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;finally we decided to use the USB protocol but do you know if I needed to program the MC9S08JM60 to be able to update the PK70FN1M0VMJ12 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank&lt;/P&gt;&lt;P&gt;MD&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2015 07:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK70FN1M0VMJ12/m-p/429386#M24813</guid>
      <dc:creator>delpymatthieu</dc:creator>
      <dc:date>2015-04-22T07:22:04Z</dc:date>
    </item>
    <item>
      <title>Re: PK70FN1M0VMJ12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK70FN1M0VMJ12/m-p/429387#M24814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Delpy,&lt;/P&gt;&lt;P&gt;Of course, you need to program the MC9S08JM60 previous, the it can work like a JTAG debug interface to the K70.&lt;/P&gt;&lt;P&gt;You'll learn more information about the OSJTAG through the link as below&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/osbdm/" title="http://www.pemicro.com/osbdm/"&gt;P&amp;amp;E Microcomputer Systems&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 02:17:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PK70FN1M0VMJ12/m-p/429387#M24814</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-05-06T02:17:46Z</dc:date>
    </item>
  </channel>
</rss>