<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: VBAT Register</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-Register/m-p/429335#M24809</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Albert&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only restriction that the VBAT register file has is that it can only store data up to 32 bytes, you just need to write directly into the VBAT register file adress: 0x4003E000.&lt;/P&gt;&lt;P&gt;Also consider it is only reset during a VBAT power-on reset and is not affected by the other reset types.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Patricia&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Apr 2015 22:00:55 GMT</pubDate>
    <dc:creator>PatriciaTeran</dc:creator>
    <dc:date>2015-04-24T22:00:55Z</dc:date>
    <item>
      <title>VBAT Register</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-Register/m-p/429334#M24808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good Mornig:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm yet doing a test of&amp;nbsp; RTC and LLWU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VBAT Register File, has some restriction?&lt;/P&gt;&lt;P&gt;I wanted to use it to store the value of the processing time. So, I am will update this register each second.&lt;/P&gt;&lt;P&gt;can be corrupted it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I implemented it on MK60FN1M0VMD12&amp;nbsp; by Keil environment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2015 14:29:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-Register/m-p/429334#M24808</guid>
      <dc:creator>albertmartin</dc:creator>
      <dc:date>2015-04-21T14:29:37Z</dc:date>
    </item>
    <item>
      <title>Re: VBAT Register</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-Register/m-p/429335#M24809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Albert&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only restriction that the VBAT register file has is that it can only store data up to 32 bytes, you just need to write directly into the VBAT register file adress: 0x4003E000.&lt;/P&gt;&lt;P&gt;Also consider it is only reset during a VBAT power-on reset and is not affected by the other reset types.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Patricia&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Apr 2015 22:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-Register/m-p/429335#M24809</guid>
      <dc:creator>PatriciaTeran</dc:creator>
      <dc:date>2015-04-24T22:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: VBAT Register</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-Register/m-p/429336#M24810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;thank you very much for the information.&lt;/P&gt;&lt;P&gt;it is very important for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; font-size: 12px; background-color: #f6f6f6;"&gt;Regards!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-size: 12px; background-color: #f6f6f6; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Albert&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Apr 2015 06:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VBAT-Register/m-p/429336#M24810</guid>
      <dc:creator>albertmartin</dc:creator>
      <dc:date>2015-04-27T06:43:56Z</dc:date>
    </item>
  </channel>
</rss>