<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FRDM-KL03Z - VREF and UART0_RX (Bootloader)</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL03Z-VREF-and-UART0-RX-Bootloader/m-p/428734#M24758</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;1. How or where in the documentation does the internal VREF get routed over to the ADC or is this intended to drive a sensor only?&lt;/P&gt;&lt;P&gt;I'd like to suggest that you can find detailed information of the VREF_OUT implement in the Chapter 30: Voltage Reference (VREF) in the KL03's reference manual.&lt;/P&gt;&lt;P&gt;And you can download it through it link as below.&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/KL03P24M48SF0RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.freescale.com/files/32bit/doc/ref_manual/KL03P24M48SF0RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/KL03P24M48SF0RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=F…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;2. If VREF can be used by the ADC, then how does one deal with UART0_RX at PTB2?&amp;nbsp; Can it be re-routed somehow?&amp;nbsp; But from what I understand the bootloader will try to use UART0 with TX/RX at PTB1 and PTB2, respectively.&lt;/P&gt;&lt;P&gt;It's not available to use the VREF_OUT and UART0_RX at the same time, you can only choose one specific function of the pin.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Jun 2015 01:46:12 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2015-06-25T01:46:12Z</dc:date>
    <item>
      <title>FRDM-KL03Z - VREF and UART0_RX (Bootloader)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL03Z-VREF-and-UART0-RX-Bootloader/m-p/428733#M24757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is a two part question:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. How or where in the documentation does the internal VREF get routed over to the ADC or is this intended to drive a sensor only?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was hoping to use the VREF as a voltage reference to the ADC, but not clear to me that it is possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. If VREF can be used by the ADC, then how does one deal with UART0_RX at PTB2?&amp;nbsp; Can it be re-routed somehow?&amp;nbsp; But from what I understand the bootloader will try to use UART0 with TX/RX at PTB1 and PTB2, respectively.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone explain this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 21:50:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL03Z-VREF-and-UART0-RX-Bootloader/m-p/428733#M24757</guid>
      <dc:creator>aes_mike</dc:creator>
      <dc:date>2015-06-24T21:50:50Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL03Z - VREF and UART0_RX (Bootloader)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL03Z-VREF-and-UART0-RX-Bootloader/m-p/428734#M24758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;1. How or where in the documentation does the internal VREF get routed over to the ADC or is this intended to drive a sensor only?&lt;/P&gt;&lt;P&gt;I'd like to suggest that you can find detailed information of the VREF_OUT implement in the Chapter 30: Voltage Reference (VREF) in the KL03's reference manual.&lt;/P&gt;&lt;P&gt;And you can download it through it link as below.&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/KL03P24M48SF0RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.freescale.com/files/32bit/doc/ref_manual/KL03P24M48SF0RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/KL03P24M48SF0RM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=F…&lt;/A&gt;&lt;/P&gt;&lt;P&gt;2. If VREF can be used by the ADC, then how does one deal with UART0_RX at PTB2?&amp;nbsp; Can it be re-routed somehow?&amp;nbsp; But from what I understand the bootloader will try to use UART0 with TX/RX at PTB1 and PTB2, respectively.&lt;/P&gt;&lt;P&gt;It's not available to use the VREF_OUT and UART0_RX at the same time, you can only choose one specific function of the pin.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2015 01:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL03Z-VREF-and-UART0-RX-Bootloader/m-p/428734#M24758</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-06-25T01:46:12Z</dc:date>
    </item>
  </channel>
</rss>