<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KL03Z32CAF4 Error Erasing flash of device</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03Z32CAF4-Error-Erasing-flash-of-device/m-p/427899#M24722</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;I solved the problem.&lt;/P&gt;&lt;P&gt;I was using a programming cable too long.&lt;/P&gt;&lt;P&gt;Thanks again&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Aug 2015 10:39:18 GMT</pubDate>
    <dc:creator>vincenzogiudici</dc:creator>
    <dc:date>2015-08-12T10:39:18Z</dc:date>
    <item>
      <title>KL03Z32CAF4 Error Erasing flash of device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03Z32CAF4-Error-Erasing-flash-of-device/m-p/427896#M24719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Hello&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;i was using a KL03Z32CAF4 to develop an application...When I launch the debugging is stopped with this error "Error Erasing flash of device"&lt;/P&gt;&lt;P&gt;what should i do?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Initializing.&lt;/P&gt;&lt;P&gt;Target has been RESET and is active.&lt;/P&gt;&lt;P&gt;CMD&amp;gt;CM C:\Freescale\KDS_3.0.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.1.5.201507151627\win32\gdi\P&amp;amp;E\supportFiles_ARM\Freescale\KL0x\freescale_kl03z32m4_1x32x8k_pflash.arp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Initializing.&lt;/P&gt;&lt;P&gt;Initialized.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;;version 1.02, 02/13/2014, Copyright 2014 P&amp;amp;E Microcomputer Systems, Inc. All rights reserved. &lt;A href="https://community.nxp.com/www.pemicro.com" target="test_blank"&gt;www.pemicro.com&lt;/A&gt; [kl_03z32k_n_pflash_m0]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;;device freescale, kl03z32m4, 1x32x8k, desc=pflash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;;begin_cs device=$00000000, length=$00008000, ram=$20000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Loading programming algorithm ... &lt;/P&gt;&lt;P&gt;Done.&lt;/P&gt;&lt;P&gt;CMD&amp;gt;EM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erasing.&lt;/P&gt;&lt;P&gt;Module could not be erased. &lt;/P&gt;&lt;P&gt;Error Erasing flash of device&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error occured during Flash programming.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PE-ERROR: Error downloading to the device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 09:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03Z32CAF4-Error-Erasing-flash-of-device/m-p/427896#M24719</guid>
      <dc:creator>vincenzogiudici</dc:creator>
      <dc:date>2015-08-10T09:44:48Z</dc:date>
    </item>
    <item>
      <title>Re: KL03Z32CAF4 Error Erasing flash of device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03Z32CAF4-Error-Erasing-flash-of-device/m-p/427897#M24720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi vincenzo giudicissi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please check your KL03 hardware at first, you should make sure your board hardware design is correct.&lt;/P&gt;&lt;P&gt;1. reset_b pin have 4.7K to 10K pullup resistor, and 0.1uf capacitor to ground.&lt;/P&gt;&lt;P&gt;2. NMI_b pin have 4.7K to 10K pullup resistor&lt;/P&gt;&lt;P&gt;3.SWD_DIO have 10K pullup&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Besides, before you download the code, did you choose the correct debug interface? Which debugger you are using?&lt;/P&gt;&lt;P&gt;Do you have JLINK debugger? You can use the JLINK , and JLINK_commander interface to check, whether it can identify the cortex M0+ core through SWD interface.&lt;/P&gt;&lt;P&gt;If can't find the core, it should be the hardware problem, if Jlink commander can find the core, then hardware have no problem, you should check the software configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check it at first, any question update information, please contact me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 02:56:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03Z32CAF4-Error-Erasing-flash-of-device/m-p/427897#M24720</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-08-11T02:56:59Z</dc:date>
    </item>
    <item>
      <title>Re: KL03Z32CAF4 Error Erasing flash of device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03Z32CAF4-Error-Erasing-flash-of-device/m-p/427898#M24721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jingjing Zhou,&lt;/P&gt;&lt;P&gt;I have checked the hardware and it is as you say.&lt;/P&gt;&lt;P&gt;In addition, the KL03 32K 24QFN I can program it ..&lt;/P&gt;&lt;P&gt;I use PEMicro Multilink Universal for debugging, and Processor Expert to set the configuration.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 07:05:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03Z32CAF4-Error-Erasing-flash-of-device/m-p/427898#M24721</guid>
      <dc:creator>vincenzogiudici</dc:creator>
      <dc:date>2015-08-12T07:05:42Z</dc:date>
    </item>
    <item>
      <title>Re: KL03Z32CAF4 Error Erasing flash of device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03Z32CAF4-Error-Erasing-flash-of-device/m-p/427899#M24722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;I solved the problem.&lt;/P&gt;&lt;P&gt;I was using a programming cable too long.&lt;/P&gt;&lt;P&gt;Thanks again&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 10:39:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03Z32CAF4-Error-Erasing-flash-of-device/m-p/427899#M24722</guid>
      <dc:creator>vincenzogiudici</dc:creator>
      <dc:date>2015-08-12T10:39:18Z</dc:date>
    </item>
    <item>
      <title>Re: KL03Z32CAF4 Error Erasing flash of device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03Z32CAF4-Error-Erasing-flash-of-device/m-p/427900#M24723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's very good to hear you solved the problem.&lt;/P&gt;&lt;P&gt;The programming cable really can't be too long.&lt;/P&gt;&lt;P&gt;Thanks for your solution sharing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 01:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03Z32CAF4-Error-Erasing-flash-of-device/m-p/427900#M24723</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-08-13T01:02:15Z</dc:date>
    </item>
  </channel>
</rss>