<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックFlash Program/Erase Cycles</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-Program-Erase-Cycles/m-p/427359#M24698</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can someone please tell me the minimum number of Program/Erase cycles for the Kinetis MCU Flash? Specifically, I'm using the KW2x. I want to avoid the EEPROM/FlexNVM option simply because it's not supported in the 512-byte MCU which we may be using in the near future.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've researched this online and found general documentation suggesting 10k-100k cycles should be expected. Is that the same across all Flash, or would each MCU be different?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Sep 2015 14:54:39 GMT</pubDate>
    <dc:creator>ignisuti_</dc:creator>
    <dc:date>2015-09-04T14:54:39Z</dc:date>
    <item>
      <title>Flash Program/Erase Cycles</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-Program-Erase-Cycles/m-p/427359#M24698</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can someone please tell me the minimum number of Program/Erase cycles for the Kinetis MCU Flash? Specifically, I'm using the KW2x. I want to avoid the EEPROM/FlexNVM option simply because it's not supported in the 512-byte MCU which we may be using in the near future.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've researched this online and found general documentation suggesting 10k-100k cycles should be expected. Is that the same across all Flash, or would each MCU be different?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 14:54:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-Program-Erase-Cycles/m-p/427359#M24698</guid>
      <dc:creator>ignisuti_</dc:creator>
      <dc:date>2015-09-04T14:54:39Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Program/Erase Cycles</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-Program-Erase-Cycles/m-p/427360#M24699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joe&lt;/P&gt;&lt;P&gt;Normally the Program/Erase cycles for the flash is defined by the technology used to create the flash, for the kinetis w family we have this information on the &lt;A href="http://cache.freescale.com/files/rf_if/doc/data_sheet/MKW2xDxxx.pdf?fpsp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;data sheet&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56850iF11744228ADC408A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt; &lt;BR /&gt;Have a great day,&lt;BR /&gt;Vicente&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 21:44:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-Program-Erase-Cycles/m-p/427360#M24699</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-09-09T21:44:41Z</dc:date>
    </item>
  </channel>
</rss>