<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: TWR-K70F120 with TWR-LCD-RGB</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427250#M24679</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Anything I can do with processor expert to drive the TWR-LCD-RGB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Ylber Doniku &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Nov 2015 13:06:06 GMT</pubDate>
    <dc:creator>donikuy</dc:creator>
    <dc:date>2015-11-24T13:06:06Z</dc:date>
    <item>
      <title>TWR-K70F120 with TWR-LCD-RGB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427248#M24677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any available eGUI project that can be used to drive the 4.3'' LCD display on the TWR-K70F120 using KDS?&lt;/P&gt;&lt;P&gt;I used to be able to run the eGUI but now I get Error: Program "make" not found in PATH.&lt;/P&gt;&lt;P&gt;Not sure what it is because it has been a while since I used this, but though might be worth starting with a fresh new up to date project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ylber&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 11:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427248#M24677</guid>
      <dc:creator>donikuy</dc:creator>
      <dc:date>2015-11-20T11:14:04Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K70F120 with TWR-LCD-RGB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427249#M24678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ylber,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, we don't have TWR-K70F120M and TWR-LCD-RGB with eGUI software based on KDS software.&lt;/P&gt;&lt;P&gt;Please check attached eGUI software for IAR software based on TWR-K70F120M and TWR-LCD-RGB boards.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 07:20:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427249#M24678</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-11-24T07:20:05Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K70F120 with TWR-LCD-RGB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427250#M24679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Anything I can do with processor expert to drive the TWR-LCD-RGB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Ylber Doniku &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 13:06:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427250#M24679</guid>
      <dc:creator>donikuy</dc:creator>
      <dc:date>2015-11-24T13:06:06Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K70F120 with TWR-LCD-RGB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427251#M24680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Porcessor Expert provides LDCD_LDD component, you can configure it to fit your needs.&lt;/P&gt;&lt;P&gt;LCDC_LDD provides general API for LCD controllers. The component provides standard features (if supported by hardware) and also special functions provided by the hardware:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Passive monochrome or color panels (CSTN)&lt;/P&gt;&lt;P&gt;TFT panels&lt;/P&gt;&lt;P&gt;Standard panel interface (1, 2, 4, 8, 12, 16, 18, 24 bit bus width)&lt;/P&gt;&lt;P&gt;Standard synchronization signals&lt;/P&gt;&lt;P&gt;Self-refresh mode&lt;/P&gt;&lt;P&gt;PWM contrast control&lt;/P&gt;&lt;P&gt;Hardware cursor&lt;/P&gt;&lt;P&gt;Hardware alpha blending&lt;/P&gt;&lt;P&gt;Hardware color keying&lt;/P&gt;&lt;P&gt;Multiple planes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LCDC_LDD component provides typical usage example at component help content.&lt;/P&gt;&lt;P&gt;Customer could refer it.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Nov 2015 05:52:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427251#M24680</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-11-26T05:52:24Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K70F120 with TWR-LCD-RGB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427252#M24681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks very much. I have added the LCDC_LDD from processor expert to the K70, but when I try to add the UserInterface errors pop up because the list processor expert gives me contains LCD controllers that I do not use. How can I add and configure the UserInterface component for the TWR-LCD-RGB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Ylber&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Nov 2015 10:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427252#M24681</guid>
      <dc:creator>donikuy</dc:creator>
      <dc:date>2015-11-26T10:13:46Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K70F120 with TWR-LCD-RGB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427253#M24682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ylber Doniku,&amp;nbsp;did you manage to work with the LDD_RGB of PE? Could you tell me how?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Diego Perea&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Aug 2017 21:52:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120-with-TWR-LCD-RGB/m-p/427253#M24682</guid>
      <dc:creator>diegoperea</dc:creator>
      <dc:date>2017-08-12T21:52:04Z</dc:date>
    </item>
  </channel>
</rss>